Skip to main content
jcrepetto
Associate II
December 27, 2009
Question

SWD (Serial Wire Debug) with ST-LINK ?

  • December 27, 2009
  • 7 replies
  • 4169 views
Posted on December 27, 2009 at 16:45

SWD (Serial Wire Debug) with ST-LINK ?

    This topic has been closed for replies.

    7 replies

    jcrepetto
    jcrepettoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    Hello,

    I have received my ST-LINK this morning, and I am wondering if it can work in SWD mode. I have tested it with the Keil and Atollic debuggers, but I can't find any configuration dialog box for the ST-LINK debug mode. Moreover, when the STM32F103ZE target is flashed with an application using the SPI3, neither GDB nor the Keil debugger can connect to the JTAG port.

    Jean-Claude

    janvi
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    While JTAG works fine, I also failed with the ''free'' atollic version for serial debug. Obviously, the ST-Link uses the same 20 pin flat cable like other download cables. If you compare with the Segger J-link, you will find very diffrent pin assignment for the 20 pin connector while others (Hitex) do not have any descriptions inside there manuals. Segger uses even pin 4-20 as ground pairs, while the ST-Link shows the ''SWIM'' connections there.

    As far as I can read in the STM32 data sheet, serial wire debug requires both, SWCLK and SWDIO for synchronous half duplex serial communication while the STM8 has a SWIM pin what is something completely diffrent. Therefore probably the truth is, that the ST-link always requires complete jtag and cannot support even the slowest software driven serial debug for the STM32.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    Cross-post:

    http://www.keil.com/forum/docs/thread16147.asp

    wiesendanger
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    I asked atollic about SWD support - here's their answer:

    The current version of TrueSTUDIO/STM32 has not support for SWD as it is not yet supported by our ST-LINK gdbserver. The reason is that SWD was not supported by the original ST-LINK JTAG device.

    However we have an updated beta version of the ST-LINK gdbserver now with SWD support that will be included in the next version of TrueSTUDIO. This require a firmware update of the sw in the ST-LINK JTAG device that we also will include in next TrueSTUDIO.

    Currently we only deliver this beta version of ST-LINK gdbserver to TrueSTUDIO PRO customers.

    Regarding JLINK the Segger gdbServer has a monitor command that shall be used to select SWD operation mode.

    Kind regards,

    Atollic support

    janvi
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    The November 09 Version 3 manual for ST-Link indicates

    ''Atollic and SWD support'' but situation is further unclear.

    With self made cable what connects SWDIO and SWCLK, the

    COM Led at the ST-Link is illuminated, but GDB server exits

    adrian239955_stm1_st
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    Just wondering, is the ST-Link working with SWD for 32-bit now? Can't find much discussion or product info to answer this question.

    EDIT

    Result! Despite the Atollic website telling me that SWD isn't supported by the Lite version I installed it anyway (seeing as it seemed to be the least crippled free IDE) and it appears to work. I thought I'd be stuck with 5-wire JTAG but this is a bonus. The ST-Link firmware updater has to be run to install the latest version (download from the ST site or as included with TrueSTUDIO) but then, when creating a project with the wizard the SWD tick-box can be selected instead of JTAG.

    Initially I connected power and all five JTAG connections to my target STM32F103RB and verified that I could conduct a standard JTAG debug session. After that I disconnected three of the wires leaving both SWIO (PA13) and SWCLK (PA14) connected. The micro datasheet explains how these two signals are used to override normal JTAG debug so I guessed they'd both be required. Note that these connections can't be made to ST-Link using the 10-way flying lead set or 4-way SWIM lead though, as this isn't SWIM.

    ersan
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    I got stuck too.

    I have an inemo v2 Board (STM32F103RE) and a ST-Link. I want access the inemo v2 Board via the ST-Link. Im using the SWD/JTAG Adapter from the iNemo V2 Board. But i cant establish a connection i always get ''no Target connected'' :(

    I need to up and download firmware to the iNemoV2 STM32F103RE chip but its not working :(

    I'cant use USB /DFU Mode i must use the SWD Header on the STM32F103

    regards

    Ersan