Skip to main content
harira
Associate
December 27, 2009
Question

USB OTG VBUS- and ID-Pin

  • December 27, 2009
  • 3 replies
  • 2366 views
Posted on December 27, 2009 at 20:01

USB OTG VBUS- and ID-Pin

    This topic has been closed for replies.

    3 replies

    chikos33
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    Good news:

    For sure, you don't need the ID pin connected since you don't use OTG mode. :)

    Bad news:

    For the VBUS pin, I think you have to connect it to the USB connector/adapter... in all cases. :(

    I hope this helps you.

    harira
    hariraAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    Hello,

    i want to use my STM32F107VC as a peripheral with virtual COM-port.

    Do i have to connect the VBUS- and ID-pin to the USB-connector?

    I need these two pins for other purposes.

    Thanks,

    C.H.

    tomas23
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:35

    The Vbus connection to PA9 is needed for two reasons:

    1. HW detecting that host is connected and the USB voltage is valid

    2. used as a reference for connecting internal 1k5 pull-up between D+ and Vbus to signal, that the device is full-speed and ready for enumeration.

    All info can be found in RefMan (RM0008).