STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error ''Invalid ROM table'' for Keil ULINK debug interface

Posted on January 05, 2012 at 15:52Hi, I have the MCBSTM32F400 development board - this worked fine up to now. Now I wanted to write some new complex application (trying to ''re-target'' a USB MSC example of ST for this board). When I loaded the new...

flyer31 by Senior
  • 5889 Views
  • 10 replies
  • 0 kudos

Issue when doing DCMI capture

Posted on January 20, 2012 at 05:12I have STM32F207 connected to the Aptina camera module. I use DCMI->DMA->PSRAM. I configured DMA in dual buffer mode to capture full resolution (5 MP). Capture is single shot. The problem I see is as follows: 1st c...

dragan by Associate II
  • 1061 Views
  • 1 replies
  • 0 kudos

uCLinux on STM32

Posted on January 18, 2012 at 18:11We were able to port the CodeSourcery uCLinux kernel for the STM3210E-EVAL to our target hardware employing an  STM32F103.  A few tweaks to the kernel source and config files were required to accomplish this feat. ...

uClinux STM32F2: Secure communications to the target

Posted on January 19, 2012 at 17:08I'd like to show in this thread how to establish a secure connection to an STM32F2 MCU using the 'dropbear' SSH daemon running on the STM32F2 target under uClinux. Ability to connect to an embedded device via a se...

STM32 I2C ''ACK Polling''

Posted on January 18, 2012 at 12:40Hi all, I need an expert advice. How to poll for ACK from addressed Slave device? The background is, if the setup has a variable count of slaves and how to get the available slaves? The second case is the M24C64 EE...

Artur1 by Associate II
  • 1004 Views
  • 0 replies
  • 0 kudos

Compilation problems for stm32

Posted on January 18, 2012 at 04:38 I have set up my toolchain under WinXP like that: 1. downloaded codesourcery LITE g++, installed it 2. downloaded Eclipse with C/C++ support 3. downloaded GNU ARM PLUGIN for Eclipse, and instal...

Why are resistors required on the boot pins?

Posted on January 17, 2012 at 10:46Hi, on the pins BOOT0, and also BOOT1 if used, the demo boards as STM32F4Discovery or others always use a resistor in line with the pin. The value varies quite much - in the AN3320 reference design, they use 10kOhm...

flyer31 by Senior
  • 2013 Views
  • 2 replies
  • 0 kudos