cancel
Showing results for 
Search instead for 
Did you mean: 

BGA64 Availability

janvi
Associate II
Posted on December 14, 2009 at 10:36

BGA64 Availability

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
janvi
Associate II
Posted on May 17, 2011 at 13:33

We have a design with very small production quantities (

The request at our STM representative resulted in F103R8H6 offer with a minimum order quantity of 3840 pieces and 12-16 weeks delivery time! Therefore I assume, the BGA64 never existed? If not, who is using a BGA64 and what is exact model ?

picguy
Associate II
Posted on May 17, 2011 at 13:33

A quick look at ST’s BGA100 & 144 shows 10mm on a side for both. Therefore you have an extra millimeter on each edge. Not the best idea. Check the size of the Luminary Micro (now TI) BGA108. If it’s 9x12 and not square the 9 side might work for you. Good luck.

gahelton12
Associate II
Posted on May 17, 2011 at 13:33

If you didn't like the LTC1661 because of setting time (30uS), then you are going to be real disappointed with the MAX5533 (660uS). :-[

Of course, the DAC in the micro has a setting time of 3-4uS. But package size and availability seems to be a major problem.

Here is another possibility for your DAC (Analog Devices AD5623RBCPZ). This is a Dual, 12 bit, serial DAC, Internal Reference, voltage output, 3-4.5uS setting time, small package.

http://www.analog.com/static/imported-files/Data_Sheets/AD5623R_5643R_5663R.pdf

Good Luck.