Posted on May 17, 2011 at 13:34Ok, thx I checked the errata. But it seems that there are no conflicts with the peripherie I want to use :-) [ This message was edited by: krk on 13-12-2009 17:40 ]
Posted on May 17, 2011 at 13:34Thanks for your quick answer. If I understand you corretly than the only thing I must consider is that two peripherals shall not share the same alternate-OUTPUT pin ?! So I would think that I can use my described scena...
Posted on May 17, 2011 at 13:34Hi, ok today I played a bit around with the STM32-P103 board ( STM32F103RBT6 ) and get confused with alternate function of the GPIO pins. I understood that I can configure each pin with the GPIOx_CRn register for his a...
Posted on May 17, 2011 at 13:33Thanks for your answers. I now looked around for a while but did not find any information if Rowley does support the ''debug under reset'' feature. Is this feature only part of the debugger or also a feature from the u...
Posted on May 17, 2011 at 13:33Hi all, I am new within the STM32 so forgive me my question ;) I am using the Olimex STM32-P103 board ( STM32F103RBT6 ) with an ARM-USB-TINY JTAG adapter and the Rowley CrossWorks IDE. My ''Hello World'' programs work ...