cancel
Showing results for 
Search instead for 
Did you mean: 

BUG? (USB_OTG_LIB)

love21cz
Associate
Posted on May 05, 2010 at 18:25

BUG? (USB_OTG_LIB)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
thomasbretgeld9
Associate II
Posted on May 17, 2011 at 13:50

Hi,

I had the same problem with the current library V3.2.1. I am using a CL device and the problem seems to be a bug in the library: Whenever you start a transfer and the last USB frame is pending, the TX Empty Fifo Interrupt is constantly asserted and the library keeps jumping into the interrupt routine until all data is read by the usb host, which usually blocks everything else. This is especially a problem if you send a packet of less then 64bytes (Max ep size in my case) and the host doesn't read it. There is nothing to reload into the fifo and the interrupt keeps triggering forever.

I found the problem in the ot_fs_int.c file in function ''static uint32_t PCD_WriteEmptyTxFifo(uint32_t epnum)''

I modified this function, which solves the problem for the moment:

static uint32_t PCD_WriteEmptyTxFifo(uint32_t epnum)

{

  USB_OTG_DTXFSTS_TypeDef txstatus;

  USB_OTG_EP *ep;

  uint32_t len = 0;

  uint32_t dwords = 0;

 

  txstatus.d32 = 0;

 

  ep = PCD_GetInEP(epnum);

 

  len = ep->xfer_len - ep->xfer_count;

  if (len > ep->maxpacket)

  {

    len = ep->maxpacket;

  }

  //Begin Modified by Thomas Bretgeld

  if ((ep->xfer_len > 0) && (ep->xfer_count == ep->xfer_len))

  {

    //Disable the Tx FIFO Empty Interrupt for this EP

    uint32_t fifoemptymsk = 0;

    fifoemptymsk = 1 << ep->num;

    USB_OTG_MODIFY_REG32(&USB_OTG_FS_regs.DEV->DIEPEMPMSK, fifoemptymsk, 0);

  }

  else

  {

    dwords = (len + 3) / 4;

    txstatus.d32 = USB_OTG_READ_REG32( &USB_OTG_FS_regs.DINEPS[epnum]->DTXFSTSx);

   

    while  ((txstatus.b.txfspcavail > dwords) &&

            (ep->xfer_count < ep->xfer_len) &&

            (ep->xfer_len) != 0)

    {

      len = ep->xfer_len - ep->xfer_count;

      if (len > ep->maxpacket)

      {

        len = ep->maxpacket;

      }

      dwords = (len + 3) / 4;

      OTGD_FS_WritePacket(ep->xfer_buff, epnum, len);   

     

      ep->xfer_count += len;

      ep->xfer_buff += len;

      txstatus.d32 = USB_OTG_READ_REG32(&USB_OTG_FS_regs.DINEPS[epnum]->DTXFSTSx);  

    }

  }

  //End Modified by Thomas Bretgeld

 

  return 1;

}

saimaddy123
Associate II
Posted on May 17, 2011 at 13:50

Hi Thomas,

May I know if you are using this for Virtual COM port and trying to transfer stdio data over USB?

Thanks,

Sai