STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Start up problem with isochronous usb transfer.

Posted on May 03, 2012 at 15:23Hello,We are two swedish students trying to implement a camera unit into a circuit board. The company we're writing this report for has developed this platform and our task is to write a protocol that handles the video...

emil83 by Associate
  • 2007 Views
  • 4 replies
  • 0 kudos

UART Rx GPIO Mode

Posted on May 06, 2012 at 21:16HiI've seen quite a few UART examples, and all of them set the RX GPIO pin as ''Input-floating''.Why is it not set to ''Push-Pull'' (which can sink and source current)? The Tx pin is set to push-pull. What is the diffe...

apatel by Associate II
  • 3088 Views
  • 3 replies
  • 0 kudos

complete reset of stm32l

Posted on May 07, 2012 at 11:55is it possible to make a complete reste oh the stm32l? because we tried to download a program, in the programme we were using the pin13 of the port A and now we can't download anything on the card. so i would like to k...

claire by Associate III
  • 1648 Views
  • 2 replies
  • 0 kudos

STM32 DISCOVERY

Posted on April 30, 2012 at 20:23Hi all I just received a STM32 discovery eval board . I am trying to learn to code new projects with it . Can you offer me a good book for this ? Thanks Elico #stm32-discovery

Mic on Discovery

Posted on May 01, 2012 at 12:37Hi. I want to simply read the PCM data coming from the microphone(MP45DT02), which is on the stm32f4 discovery board. I configured the I2S2_CK and I2S2_SD pins, the I2S communication, and enabled the SPI_I2S_IT_RXNE in...

I2C

Posted on October 21, 2010 at 16:50hi i am tring to activate the I2C in order to External EEPROM i used this code but nothing is in the output on PB why? #include ''stm32F10x.h'' #define IWDG_WriteAccess_Enable     ((uint16_t)0x5555) #define IWDG_Pr...

ezrab by Associate II
  • 4251 Views
  • 12 replies
  • 0 kudos

SPI2 won't work

Posted on May 03, 2012 at 12:08 Hi, I've been trying to solve this problem for quite a while now. I 've get throuth various forum or example projet but nothing do the trick . My stm32f107 is connected by spi with another microchip (b...

STM32F207 Usart TX-RX with Parity_even

Posted on May 01, 2012 at 15:20Dear all, I'm in trouble with usart to communicate with a peripheral that use parity even. I'm working with STM32F207 and I have an RS485 transceiver I have configured the usart as below: void USART3_Config (void) {   ...

momede by Associate II
  • 1592 Views
  • 2 replies
  • 0 kudos