STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C

Posted on October 21, 2010 at 16:50hi i am tring to activate the I2C in order to External EEPROM i used this code but nothing is in the output on PB why? #include ''stm32F10x.h'' #define IWDG_WriteAccess_Enable     ((uint16_t)0x5555) #define IWDG_Pr...

ezrab by Associate II
  • 4296 Views
  • 12 replies
  • 0 kudos

SPI2 won't work

Posted on May 03, 2012 at 12:08 Hi, I've been trying to solve this problem for quite a while now. I 've get throuth various forum or example projet but nothing do the trick . My stm32f107 is connected by spi with another microchip (b...

STM32F207 Usart TX-RX with Parity_even

Posted on May 01, 2012 at 15:20Dear all, I'm in trouble with usart to communicate with a peripheral that use parity even. I'm working with STM32F207 and I have an RS485 transceiver I have configured the usart as below: void USART3_Config (void) {   ...

momede by Associate II
  • 1607 Views
  • 2 replies
  • 0 kudos

Please help me to undersand how USB FIFO in STM32F4 work

Posted on May 03, 2012 at 22:09Hello all, this is my first discussion here. I'd like to write my own software to control USB in STM32F4 device using bulk transfesr in peripheral mode only. I read USB ON-The-Go chapter in Reference Manual thoroughly ...

kekon1234 by Associate III
  • 912 Views
  • 0 replies
  • 1 kudos

STM32F3210E-Eval not responding via JTAG

Posted on May 02, 2012 at 16:31Hi,we are using three STM32F3210E-Eval for about 1 year now. Recently 2 of these boards stopped responding via JTAG. The JTAG interface used is a Segger J-Link Edu. Different J-Links on different PCs have not made a di...

Usart Polling

Posted on April 13, 2012 at 13:28Hi, why i have to enable USART1->CR1 |= USART_CR1_RXNEIE; for polling In Example of ST Lib i dont see such thing. I thought for polling i dont need this?

STM32F207 Usart DMA RX Interrupt

Posted on April 26, 2012 at 21:20dear all, I'm working with the microcontroller STM32F207, below there is my function to configure the DMA in order to acquire 3 characters from USART2 and have the interrupt when those 3 characters arrived. Unfortuna...

momede by Associate II
  • 1503 Views
  • 2 replies
  • 0 kudos