STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI reception, data shifted by one bit

Posted on June 08, 2012 at 17:42Hi,I am having some difficulty receiving SPI data correctly and I am hoping someone could help.I currently have two STM32L-Discovery boards connected via SPI with one acting as master and one as slave. My SPI transmis...

gavin2 by Associate II
  • 876 Views
  • 0 replies
  • 0 kudos

STM32 USB Host Device Library v2.1.0 with F4 support

Posted on April 03, 2012 at 19:57Hi all,I don't see this mentioned anywhere on the forum, but a new version of the STM32 USB library was released recently and it adds the long-awaited support for the STM32F4 family. I've tried it with the STM32F4-Di...

tony2399 by Associate II
  • 3645 Views
  • 8 replies
  • 0 kudos

Synchronized (Chained/Cascaded) Timers

Posted on June 06, 2012 at 18:13Newbie here...I'd like to use one timer as a prescaler for another. Both these timers (combined) will act like a single 48-bit ''uptime'' value, used for timestamping events. The master timer will be driven off APBx.I...

sacleary by Associate II
  • 1442 Views
  • 2 replies
  • 0 kudos

How to store user data in flash memory(stm32f207ig)

Posted on June 05, 2012 at 16:28Hello All,I have been trying to write into the flash(certain user data), but when i debug it i see the values being written elsewhere in other locations and sometimes in the location i have specified.The function i ha...

issue of reading RTC

Posted on June 06, 2012 at 08:48Hi All,I am wondering if there is an internal interlock that prevents the RTC from being updated while the registers (RTC->CNTH and RTC->CNTL) are being read.There is a situation where RTC->CNTH has been read RTC then...

markaren1 by Associate II
  • 1098 Views
  • 1 replies
  • 0 kudos

Starting with a STM32F100CBT6B

Posted on June 05, 2012 at 21:30Hello, I am new to ST micros and this is my first attempt to design a board based on a 32-bit microcontroller. I've designed a very simplistic circuit with all of the GPIO ready for use for experimenting with breadboa...

gmwralhs9 by Associate II
  • 2387 Views
  • 4 replies
  • 0 kudos

gdb backtrace/ exception handlers

Posted on May 24, 2012 at 20:20Very occasionally, my code takes an unexpected exception and ends up in a default handler :)I'd like to write such a handler so that GDB can successfully unwind the stack.  For example,default_handler (void) { asm(''ld...

USART3 interrupts - stm32f4xx

Posted on June 04, 2012 at 05:32Anyone have any example code for USART Interrupts? I've tried finding some example code to work off of. 

spyguy99 by Associate II
  • 2843 Views
  • 7 replies
  • 0 kudos