Posted on May 17, 2011 at 14:05Thanks Duncan,I have already tried the code which u have sent , then the problem which i am facing is...In the reset i used the code which u have sent, and in my send function after toggling(DTOG_RX) i used the SetEP...
Posted on May 17, 2011 at 14:01Thanks for the replies, one interesting thing i am seeing in the map file generated.These are the observations when the ''user symbols case sensitive'' option is checked and uncheked..1) When Checked, i.e in the no iss...
Posted on May 17, 2011 at 14:01Some more debugging that i have done on this..My code is going to the main , from there if i step in many times then its not showing the Hard Fault exception , but when i just do go its showing that, i tried stepping i...