cancel
Showing results for 
Search instead for 
Did you mean: 

Two channels of same timer to output two shifted pulses

nchristoforou
Associate
Posted on August 11, 2010 at 22:27

Two channels of same timer to output two shifted pulses

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
swhite2
Associate III
Posted on May 17, 2011 at 14:01

I'm pretty sure that's not possible with a single timer.Even with two timers I'm not sure, offhand, whether you can synchronized them to your requirements.

kashif
Associate II
Posted on May 17, 2011 at 14:01

it is not possible to start second pulse ''exactly'' when the first pulse ends but the SHIFT can be minimized with some custom code. have a look at RM0008 reference manual > Timer Synchronization (article 13.3.15 - page 296)

hope it helps. regards.

nchristoforou
Associate
Posted on May 17, 2011 at 14:01

(...After some time working on another project). Thank you for your replies. I did look at the ''Timer Synchronization'', but unfortunately, this talks about using one timer to trigger another, something that I could see how to do it.... here we want one channel to trigger another from the same timer. My feeling is that this cannot be done. I just need to convince my hardware engineer who designed it that way ;)