STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART4 interrupts during emulation break

Posted on June 27, 2012 at 11:19Hi, I am using the Keil ARM MDK development tool with an STM32F103ZG microcontroller and ULINK Pro JTAG. I have some UART code that I would like to test which requires the generation of UART transmit and receive inter...

dsjnews by Associate III
  • 1959 Views
  • 4 replies
  • 0 kudos

how to use STM324xG-EVAL projects on STM32F4 discovery board

Posted on June 09, 2012 at 20:15how to use STM324xG-EVAL projects on STM32F4 discovery board????friends i am new to discovery board...nd i want to use SDIO of discovery....bt example progrms for discovry doesnt contain SDIO program bt for STM324xG-E...

rishi by Associate II
  • 2106 Views
  • 4 replies
  • 0 kudos

How to disable the write buffer(ACTLR ,DISDEFWBUF)

Posted on June 27, 2012 at 13:16Basically my application goes into the hard fault handler(where the IMPRECISERR bit is set) and I have read up about this on some forums and found out that I cannot find out the exact instruction causing this fault Ho...

notation

Posted on June 27, 2012 at 14:51Whats the difference about NVIC_SetPriority(TIMER0_IRQn, ((0x01<<3)|0x01)); and NVIC_SetPriority(TIMER0_IRQn, 9);   Is There a special motive to use the first form?????? THANKS #notation

esiqueira by Associate II
  • 1154 Views
  • 2 replies
  • 0 kudos

USB, DMA, CDC and Speed ... Is it possible?

Posted on June 25, 2012 at 23:05Hi all, I have a fair bit of experience with the STM32 now and have got most peripherals working as I want on multiple projects but I am yet to master the USB. I would like to transfer data collected by a series of ...

gareth2 by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos

Olimex STM32-P407 USART3

Posted on June 23, 2012 at 13:55Hello,After dealing with my code for two days I have no other option than ask you guys. I have problems with my USART3/6 serial port on my Olimex STM32-P407 board:http://www.olimex.com/dev/pdf/ARM/ST/STM32-P407 Initia...

StdPeriph_Driver I2C

Posted on November 30, 2011 at 12:01Hello all, I want to use the StdPeriph_Driver as a guide for my own project. Part: STM32F100RB value line discovery (test kit). Trying to get the I2C to work. I want to use the I2C files (.c+.h) for my own projec...

STM32F4, Weird behavior with TIM6 to blink an LED

Posted on June 25, 2012 at 06:08I'm trying to learn how to use the basic timers, without the benefit of a library, so I have been reading the RM0090 reference manual. As a simple test I want to toggle the blue LED on the dev board (pin D15) once per...

upgrdman by Associate II
  • 1497 Views
  • 2 replies
  • 0 kudos

Discovery - disabling onboard peripherals

Posted on June 26, 2012 at 03:38Hi, Bit of a noob question here, but I'm planning to use a STM32F4DISCOVERY board purely for its onboard programmer and also to save space on my PCB (will connect via header). Unfortunately this means i get a bunch of...

GCC based Linker file for the STM32F0

Posted on June 26, 2012 at 18:26 Hello all I just wrote a simple linker file to be used in the gcc environment. One of my goals was to define a stack and heap section in the linker file. The linker file is provided below. It seems to compile wit...

halherta2 by Associate II
  • 1427 Views
  • 1 replies
  • 0 kudos