STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART1 simple use problem

Posted on June 29, 2012 at 10:24Hello everybody, I begin with CortexM4 STM32F4 on a keil developpement board (MCBSTM32F400) I try to use USART1 in a very simple mode. I take a look to example and discuss forums. My config seems to be good but no sig...

Beginner with ADC3_DMA, ADC3ConvertedValue constant

Posted on June 28, 2012 at 01:21using gcc 4.5.2, st-util 4242, stm32f4discovery, ADC3_DMA peripheral examples from STM32F4-Discovery_FW_V1.1.0, ld file from TrueStudio, startup file from CMSIS. When I run the program in the debugger the ADC value do...

STM32F4 TIM1 PWM missing ch1..3

Posted on June 28, 2012 at 17:48 STM32F4 TIMER 1 PWM1. Please can someone tell me how to enable channels 1, 2 and 3. Channel 4 is fine generating a PWM at 0..100% at 20Hz. I know channels 1..3 hardware is different - just can't figure out what t...

John F. by Senior
  • 1541 Views
  • 3 replies
  • 0 kudos

PWM on PB.10 and PB.11 with DMA and TIMER2(CH3 e CH4)

Posted on June 28, 2012 at 19:38How can I configure PWM on TIMER2 (CH3 and CH4)? I would like to configure CH4 in other Channel of the DMA, but looks that only run on Channel 2. /* Configuracoes DMA */  DMA_DeInit(DMA1_Channel2);  DMA_InitStructure....

esiqueira by Associate II
  • 1263 Views
  • 2 replies
  • 0 kudos

HSI and GPS interference

Posted on June 28, 2012 at 01:33 Hello everyone, Did anyone notice that STM32 with an internal HSI at 8MHz cannot be used in proximity to an embedded GPS antenna? The 8MHz internal oscillator happens to have the 197th harmonic close to L1...

michele77 by Associate II
  • 1791 Views
  • 3 replies
  • 0 kudos

Timer Preload and Shadow registers

Posted on June 28, 2012 at 12:38Hi, I am trying to get a better understanding of the timer hardware for the advance control timers. In section 14.3.1 of RM0008 (Rev. 14) it states:- ''The auto-reload register is preloaded.Writing to it or reading fr...

dsjnews by Associate III
  • 3121 Views
  • 4 replies
  • 1 kudos

STM32F107VC CAN bus pin remap

Posted on June 20, 2012 at 23:19hi.i am using the STM32F107VC board from IAR i have some example code for CAN but in my Board they used the PD0 and PD1 for CAN i dont know how to remap it in my code. i have 2 board and i want to sent data between 2 ...

hello by Associate II
  • 5542 Views
  • 20 replies
  • 0 kudos

Max data speed into STM32F4 Discovery via the STLink/V2

Posted on June 27, 2012 at 01:07I was looking to use the STM32F4 Discovery board as an output device which requires a significant bandwidth from the supporting PC.  I don't have specifics nailed down on this task, 115.2Kbaud might be sufficient but ...

dannym by Associate III
  • 3172 Views
  • 5 replies
  • 0 kudos

SDIO can't read more than 511 blocks

Posted on June 26, 2012 at 22:41I'm using the standard STM libaries. I'm using SDIO with DMA. It works perfectly when reading up to 511 blocks but as soon as I try and read 512 blocks it stops working. It would successfully transfer 511 blocks then ...