STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sprintf issue on STM32F4xx serie

Posted on June 26, 2012 at 12:09Hi, I am converting from STM32F205 to STM32F405 and have an issue with printf. I have updated the �C Library, use FPU, and updated OpenRTOS. Are there some settings that I need to change to make printf to work with th...

kai239955 by Associate II
  • 1009 Views
  • 1 replies
  • 0 kudos

STM32F4-Discovery resets

Posted on June 22, 2012 at 12:29 I've wiredSTM32F4-Discovery board and USB<->UART and wrote a little program that prints ''r'' in the main function. There's the initialization code for USART. In terminal I can see letter ''r'' coming every hal...

timon1994 by Associate II
  • 1742 Views
  • 5 replies
  • 0 kudos

stm32f10x DMA RX Interupt ....

Posted on June 18, 2012 at 07:40HI I want to use DMA to Recieving data via uart (rs485)  I want to use 20byte buffer but for siplicity in this exaple is shown only 1byte buffer...  int main(void){  RCC_Configuration();  GPIO_Configuration();  USART...

redkofka by Associate II
  • 1448 Views
  • 2 replies
  • 0 kudos

Document RM0038 is missing figure 209

Posted on June 25, 2012 at 19:25Document RM0038, or CD00240193.pdf, the reference manual for the STM32L1xx, revision 5, is missing figure 209 on page 589/809.I can see figure 208 just fine but I can't see figure 209I would like to see it to help me ...

USART1 Very Low Output Signal

Posted on June 13, 2012 at 12:15Hi,I am doing what on paper should be one of the simplest tasks possible with a USART - namely configuring it and then getting it to output a pattern using USART_SendData();When I send this command it is definitely do...

dclark9 by Associate II
  • 2173 Views
  • 6 replies
  • 0 kudos

lsm330dl output read problem

Posted on June 19, 2012 at 16:50hi, everyone. i don't understand why the output data XH,XL. is unchange all the time , when i  read the status_reg, i find that there is no new data coming ..and sometimes the same code gave me different output ,like ...

How to reduce the project size.

Posted on June 23, 2012 at 20:56hi,i have the project from IAR Embedded workbench when i try to compile it size code exceed,, i am using only code size limited.this project have lot of function like LCD, Temp sensor, USART, ect..now i am just trying...

hello by Associate II
  • 2426 Views
  • 3 replies
  • 0 kudos