Posted on May 28, 2013 at 22:42
Take a look at the video below, which shows Linux, in its uClinuxform, running on the STM32F437 microcontoller:
http://www.youtube.com/watch?v=_uO8KfhfY2Y&feature=youtu.be
The novelty of this con...
Posted on February 02, 2012 at 12:20Here is a sample session showing some basic uses of SNMP for remote management of an STM32-based device. This session was run under uClinux on an STM322G-EVAL board with Emraft's STM-MEM add-on. (Refer to www.emcr...
Posted on January 19, 2012 at 17:08I'd like to show in this thread how to establish a secure connection to an STM32F2 MCU using the 'dropbear' SSH daemon running on the STM32F2 target under uClinux. Ability to connect to an embedded device via a se...
Posted on April 19, 2012 at 08:21Emcraft Systems has open sourced its ports of U-Boot and uClinux for Cortex-M3 and Cortex-M4 at github:https://github.com/EmcraftSystemsFor more information about supported reference platforms, refer to Emcraft's web...
Posted on January 19, 2012 at 17:14Please check this http://www.emcraft.com/index.php/products/89. This uClinux port supports pthread-style multithreading on STM32F2.
Posted on January 14, 2012 at 20:38Indeed, Emcraft Systems provides Linux (uClinux) port for STM32F2 using the STM3220G-EVAL board + Emcraft's STM-MEM add-on as a hardware reference platform http://www.emcraft.com/index.php/products/89. The STM-MEM...