STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spi interrupt problem for lsm330dl

Posted on July 09, 2012 at 12:33i try to use the spi interrupt , but the whole program just hanged at case 101 which is in the void GYRO_Task(void),  it shows me ''+++''. anything wrong? here is some part of my code.  #ifdef GYRO_SPI_USE_INTERRUPT  ...

Conflict with two EEPROM

Posted on July 06, 2012 at 10:02Hi, With a STM32, I have a problem to select either EEPROM (M24LR64-R and M24M02-DR) on the same bus I2C. Here are the ''device select code'': For M24LR64-R:  1 0 1 0     X 1  1 X In the order:  1 0 1 0 = Device ...

does debugging erases data eeprom?

Posted on July 15, 2012 at 12:07Hi, I am using the discovery board (stm32l) using gcc and the gdbserver from Atollic. My program can erase the data eeprom and write some new values in it, However when I start a new debug session the contents seems t...

wdehoog by Associate
  • 770 Views
  • 0 replies
  • 0 kudos

USB Host Firmware and STM32 - Pay or Free

Posted on July 11, 2012 at 15:39 Hello ALL We have already completed a project with the STM32F It took some time to get up to speed but eventually we did, and completed a complex project. Now we have a project which could work with a s...

dgleeson2 by Associate II
  • 2266 Views
  • 4 replies
  • 0 kudos

TIMER (Duty and OCActive)

Posted on July 11, 2012 at 15:46Hi, I would like to know why in TIM_OCMode_PWM1, I can calculate the frequency 'Duty cicle'                         TIM_CLK / (TIM_Period + 1)                36MHz/(999+1)  Frequencia  =  -----------------------------...

esiqueira by Associate II
  • 1909 Views
  • 2 replies
  • 0 kudos

TIM_ClearFlag() function in stm32f10x library

Posted on July 07, 2012 at 09:02The content of this function is /* Clear the flags */   TIMx->SR = (uint16_t)~TIM_FLAG; But I think it must be in this format: /* Clear the flags */   TIMx->SR &= (uint16_t)~TIM_FLAG; a & is needed for correct clear ...

Boundary Scan on STM32F1 µCs

Posted on July 13, 2012 at 10:56Dear ladies and gentlemen, I am currently writing on my Bachelor thesis about boundary scan and its advantages/ disadvantages. Our company is currently launching the new STM32 micro-controller family and it is my task...

issue with stvp

Posted on July 03, 2012 at 13:44Hi, As you can see from the schematic below,the ''C3'' capacitor is a low voltage 1.5F supercap that I use as backup battery to keep the mcu up during the stand-by mode. My problem is that,while I flash the program me...

0690X0000060513QAA.png