Posted on December 07, 2011 at 17:11People here could help others, instead of loosing everybody time with useless posts.I had the same problem, solved enabling the Ethernet clocks only AFTER while(ETH_GetSoftwareResetStatus()==SET).Why? Read the STM...
Posted on June 09, 2011 at 19:00I could successfully download following these steps: Download the Flash Loader Demonstrator v2.2.0. Use a USB2UART IC (I use FT232RL), or RS232 driver with DTR and RTS. Use DTR as NRST and RTS as BOOT0. Configure...
Posted on May 17, 2011 at 14:07Aly,Some weeks ago I did the same as you, but ST did not answered yet.Keil has released MDK 4.13a. Look one of the updates:Updated: support for ST-Link USB-JTAG debugger. The ST-LINKIII-Keil.dll MDK driver in folder .....