Interrupts unexpectedly fired!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2010-09-15 10:16 PM
Interrupts unexpectedly fired!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:07 AM
I don't like the order you initialize things, the clocks to the peripherals, including GPIOD, need to be up and running before you prod the hardware. It is after all synchronous.
uint8_t CAN1_Init(void) { uint8_t retVal = CANINITFAILED; // Initialize clocks into hardware BEFORE configuring them! // Enable CAN 1 Clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); // Enable AFIO and GPIOD clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOD, ENABLE); CAN_DeInit(CAN1); GPIO_InitTypeDef GPIO_InitStructure; // Configure CAN Tx (PD.01) as push-pull GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOD, &GPIO_InitStructure); // Configure CAN Rx (PD.00) as input floating GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOD, &GPIO_InitStructure); // Remap CAN1 to PD0 and PD1 AFIO->MAPR &= ~(AFIO_MAPR_CAN_REMAP); AFIO->MAPR |= AFIO_MAPR_CAN_REMAP_REMAP3; // Configure for 1MBit CAN_InitTypeDef ci; CAN_StructInit(&ci); ci.CAN_Prescaler = 4; ci.CAN_SJW = CAN_SJW_1tq; ci.CAN_BS1 = CAN_BS1_6tq; ci.CAN_BS2 = CAN_BS2_2tq; ci.CAN_TXFP = ENABLE; retVal = CAN_Init(CAN1, &ci); if(retVal != CANINITFAILED) { NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); // 1:3 // Tx Interrupt channel NVIC_InitStructure.NVIC_IRQChannel = CAN1_TX_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // Peripheral tx interrupt enable CAN_ITConfig(CAN1, CAN_IT_TME, ENABLE); } return retVal; }Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:07 AM
Yeah, that is probably a good point. Actually the GPIOD and AFIO clocks are already up and running from previous peripherals and I should of removed the AFIO clock init function call. The CAN clock is enabled before any access to the CAN peripherals registers.
Anyways, that doesn't really answer my questions about the interrupts as in practice all clocks are up and running and I did retry it after moving the CAN clock init to earlier and the same thing still happens...