STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to cascade Encoder and Input Capture Mode

Posted on July 24, 2012 at 19:04General Purpose Timer 4 counts the position from incremental encoder in quadratur mode. The Encoder has 200 slots and for low speeds, the frequency is rather low. To derive the rotation speed, I subtract 2 positions i...

jveith by Associate II
  • 1079 Views
  • 0 replies
  • 0 kudos

I2S fullduplex with DMA (stm32f407)

Posted on March 07, 2012 at 15:22I configure SPI2 and I2S2_ext for running I2S in fullduplex mode using DMA1_Stream4 and  DMA1_Stream2. DMA1_Stream4_IRQHandler called and i2s tx is working fine, but DMA1_Stream2_IRQHandler not called at all. Please ...

uuftc by Associate
  • 2773 Views
  • 5 replies
  • 0 kudos

STM32F407VGT6 and I2S

Posted on July 16, 2012 at 18:06Hi all!!!Please help me. A have problem with I2S interface in this MC. I need to work with audio codec cs4221 by means of I2S. I setup I2S2 interface in full-duplex mode (I2S2- Master reciev, I2S2ext - Slave TX). Data...

rx9cim by Associate II
  • 2853 Views
  • 5 replies
  • 0 kudos

Olimex STM32F207 , no text on the LCD display

Posted on July 16, 2012 at 11:22Hi, I am new to LCD display controller. I am using Olimex STM32F207 board with onboard 6610 LCD color 128x128 TFT display. I have initialized the LCD according to Example code. I my case I could see LCD backlight is ...

skdeka by Associate II
  • 1208 Views
  • 2 replies
  • 0 kudos

IWDG DBGMCU

Posted on July 02, 2012 at 15:01Hi, I  am using IWDG and it works good. I would like to stop it when core halts (in breakpoints), therefore i did:   DBGMCU->CR |= DBGMCU_CR_DBG_IWDG_STOP; But it does not stop the IWDG. Do i miss something? Thanks.

ybitton by Associate II
  • 1264 Views
  • 1 replies
  • 0 kudos

Programming the STM32F4

Posted on July 17, 2012 at 05:01Hi, I originally was planning on using the Discovery demo board, but have since changed to placing the MCU directly on my PCB. Now what is the easiest way to program the thing? The Discovery uses a STM32F103C8T6, per...

Does anyone have a quick and dirty i2c example?

Posted on November 22, 2011 at 00:18Hi all, I am very new to the STM32, currently using the STM32L.. As I am new to developing on this platform (Never touched anything ARM before), I am overwhelmed by the amount of documentation although trying to ...

STM32F4 and TFT 3.5'' SSD1963

Posted on July 16, 2012 at 10:01Hi all! I connected STM32F4 board to a LCD 3.5'' TFT with SSD1963 driver and FSMC controller. I wrote some code like this:http://www.mediafire.com/download.php?v762hz2pdxxxlz1 but the screen like a TV when I disconnec...

mdphuong by Associate
  • 1867 Views
  • 2 replies
  • 0 kudos