STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing OV2640 sensor with stm32f103

Posted on August 10, 2012 at 13:53How to enable single snapshot mode in ov2640 sensor....i want to take a single image & then store it to SD card.......can ne1 pls help me out....Thanks

pawan by Associate
  • 842 Views
  • 0 replies
  • 0 kudos

STM32F41G-EVAL Ethernet 100MBit/s

Posted on August 10, 2012 at 11:56Hi, im using the stm32f41ig-eval board an i modified the example: STM32F4x7_ETH_LwIP_V1.0.0/ FreeRTOS httpserver_socket. After the modification i can send data to the server an it send it back to the client. Than i...

ingo2 by Associate
  • 718 Views
  • 0 replies
  • 0 kudos

stm32 discovery, usart not working at all ?

Posted on August 06, 2012 at 04:27I had tried to move a working application to my stm32 discovery 'b'. I defined it as STM32F10X_LD_VL and am using the latest libraries from the stdperiph. The usart does not work at all (no high/low on scope). I had...

ILI9325 without fsmc white screen problem

Posted on August 09, 2012 at 21:04Hi, i am using stm32f103rbt6 (a known board model called stm-mini), but i have some problems with this hardware. I am sure the stm is fine the problem is the ILI9325 lcd. First, all worked fine. So i started to load...

jltellop by Associate
  • 797 Views
  • 0 replies
  • 0 kudos

USB3340 from SMSC allways working in FS usin a STM32F407

Posted on August 01, 2012 at 18:11Hi All, I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3...

angel2 by Associate
  • 1410 Views
  • 2 replies
  • 0 kudos

STM32F4 I2C Issue?

Posted on May 23, 2012 at 18:47At a high level, I'm able to get I2C on the STM32F4-Discovery board working with our part (MAX5418), but there's one problem I'm having, and that is that I have to write commands twice in order for them to be received....

Random code hangs

Posted on August 07, 2012 at 19:42HelloI dont know why, but when I use FFT code, STM32F103RBT6 just stop running in totally different part of code - mostly in parts of STD library where asserts are defined. So I think it can corrupt memory or someth...

zexx86 by Associate II
  • 2294 Views
  • 4 replies
  • 0 kudos

F0 Discovery - fprintf function implementation

Posted on August 02, 2012 at 22:05Wondering if anyone in the forums has made an fprintf function or equivalent?  I got characters spitting out to hyperterminal, now just trying to figure out to spit out variable info to the screen.

wbarkley by Associate II
  • 1372 Views
  • 6 replies
  • 0 kudos

How to escape USART1 interrupt?

Posted on August 06, 2012 at 22:51Below is my USART1 handler: void USART1_IRQHandler(void) {     if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET){         USART_SendString(USART1, ''\r\n======Blow ME======\r\n'');         USART_ITConfig( USART1...

wbarkley by Associate II
  • 1877 Views
  • 4 replies
  • 0 kudos