STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with configuration I2S interface

Posted on August 13, 2012 at 15:06Hi everybody! I used external codec ADAU1961 for collect data from two microphones. I used I2S3 simplex mode for receiving data from codec to STM32F4. I configured lines of peripheral I2S3 for transmition (WS - Word...

krzkrok by Associate II
  • 2391 Views
  • 4 replies
  • 0 kudos

Electromagnetic protection for JTAG interface?

Posted on August 10, 2012 at 13:41Hi, im not sure if this is the correct subforum for this question, if not please move this subject to the correct spot. I am wondering if it is necessary to protect the JTAG interface of the STM32 processors from el...

Puzzled by USART behavior

Posted on August 14, 2012 at 21:32I'm porting over some code that I previously ran on Stellaris hardware to an F4Discovery board. I hooked a logic analyzer up to take a peek at what my USART code (with hardware flow control) was doing and found some...

andyturk by Associate II
  • 1889 Views
  • 4 replies
  • 0 kudos

Multiple software reset conditions.

Posted on September 09, 2011 at 10:35Hello,I'm developping an application with bootloader. Today I'm using USART1 to communicate with the host PC, and I'm using a software reset to enter bootloader mode on demand (bootloader check if it's a software...

root by Associate II
  • 1484 Views
  • 6 replies
  • 0 kudos

Powering STM32F4-Discovery from micro usb

Posted on August 14, 2012 at 03:05I'm looking to power the STM32F4 discovery from the micro usb port, while keeping modifications to the board at a minimum (I don't have great faith in my smd soldering).This is my current idea:- remove r46 to ensure...

devin122 by Associate
  • 1842 Views
  • 2 replies
  • 0 kudos

STM32F4DISCOVERY - PC0 and PB2 pins

Posted on August 08, 2012 at 21:30Hi,     I would like to have some more information in regard of the PC0 pin on the STM32F4Discovery. I read on the forum that quite some people use this pin as an adc channel, but on the User Manual I can see that i...

guitest02 by Associate II
  • 3024 Views
  • 3 replies
  • 0 kudos

F4 Discovery Max SPI Speed

Posted on August 11, 2012 at 02:46Hello,1. What is the maximum SPI speed I am suppose to achieve with the 8MHz HSE? 2. I would like to achieve at least 25MHz, what would it take to achieve that both code and HW? Currently with my code below I get 13...

jvaldez by Associate
  • 1459 Views
  • 2 replies
  • 0 kudos