cancel
Showing results for 
Search instead for 
Did you mean: 

VBAT_Mesurement STM32V207 unusual results

hhosburg
Associate II
Posted on May 08, 2012 at 18:13

Hello,

I've used the code from the example VBAT_Mesurement to test the ADC. Instead of connecting a  battery on pin VBAT I've connected VDD 3.3V.

The program requests cyclic the converted value.

....

VBATVoltage = (ADCConvertedValue*2)*3300/0xFFF;

...

VBATVoltage  varies from 3287 to 2992. this is a difference  about 8 percent.

I've checked the power VDD with an oscilloscope , which  is quit clean.

There are no peaks visible.

Does anybody know the reason for this ?

Regards,

Harald

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on May 08, 2012 at 21:44

Does anybody know the reason for this ?

Using 15 cycle mode I'm seeing +/- 20%, this drops below +/- 1% in 480 cycle mode.

ADC_SampleTime_480Cycles

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hhosburg
Associate II
Posted on May 09, 2012 at 07:36

Thanks,

it works

Harald