STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 CPU Configuration Software

Posted on October 29, 2012 at 14:28hello,everyone, I'm developing a STM32F4 CPU configuration software. It can be used to configure pins and to write configuration ''C'' code for you. Please waiting.........

0690X00000602mVQAQ.jpg

unsigned_int and unsigned_short_int compatibility ?

Posted on October 30, 2012 at 13:32 Hi there, May be this is a silly question, but could someone explain me to how we use unsigned int and unsigned short int types together ? Here is an exemple from a simple working code (gpio.c* of STM32 V...

edgar2 by Associate II
  • 1856 Views
  • 2 replies
  • 0 kudos

Cannot set EXTICR register in STM32F205

Posted on June 21, 2012 at 00:14 Following the example for the STM3240G I set up the KEY pushbutton (PG15) as an external interrupt: RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); // enable port RCC_APB2PeriphClockCmd(RCC_APB2Peri...

TimerX chain or master example

Posted on October 30, 2012 at 10:10I want to measure distance between two pulses, pulses come from an another timer. Ist there any example for it? #timer-master-slave

stst9184 by Associate II
  • 964 Views
  • 3 replies
  • 0 kudos

STM32F4Discovery VCP Problem

Posted on October 29, 2012 at 01:55Hello, I am trying to add VCP on STM32F4Discovery but have some issues which I am not able to figure out. When I add this command USBD_Init(&USB_OTG_dev, USB_OTG_FS_CORE_ID, &USR_desc, &USBD_CDC_cb, &USR_cb); in ...

measuring of execution time

Posted on October 28, 2012 at 20:05Hi everybody. Is it possible to measure execution time of program when I debug the program by using of hardware debugger ST-LINK V/2? I use uVision 4 studio (lite version) by KEIL and discovery board for STM32f0 wi...

Timer Interrupt frequency influenced by WFE

Posted on October 29, 2012 at 02:03Dear readers, the attached program for the STM32F407VGT6 (on the STM32F4 Discovery) should generate an interrupt every 500ms. The ISR toggles GPIO pin D14, which lets the LED (red) connected to it blink with 1Hz. T...

profclonk by Associate II
  • 1371 Views
  • 2 replies
  • 0 kudos

STM32F107RCT6 (LQFP64) - JTAG Help!

Posted on October 27, 2012 at 19:35Hey Guys: Please take it easy on me, I am a rookie STM32 user. I've recently ''adopted'' a new project from my employer due to the old engineer leaving the company abruptly.   I've been tasked with flashing several...

i2c start doesn't do anything on the bus

Posted on October 28, 2012 at 17:18 I am trying to write an i2c driver for my stm32f100 discovery board. To verify that it is setup right, I want to send a start condition and check to see that the SDA line goes low while SCL stays high. I have ...

saccrue by Associate II
  • 832 Views
  • 2 replies
  • 0 kudos