STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

StdPeriphLib Question

Posted on November 01, 2012 at 17:29So does the whole family of STM32M0-STM32M4 have their own StdPeriphDriver offering?  Under the advisement of my hardware guide, I am trying to test out the Freescale Freedom board after I have developed on the ST...

wbarkley by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

Bus Fault occured randomly during normal operation

Posted on November 01, 2012 at 07:44Dear all, MCU we are using is STM32 F103CBT6, on a motor driver application. Wehave encountered a strange phenomenon that Bus Fault occurred randomly duringnormal operation, and the fault message shows that the PC...

edison72 by Associate
  • 1098 Views
  • 1 replies
  • 0 kudos

DMA: Reset hidden increment registers

Posted on October 31, 2012 at 08:05I emulate an I2C eeprom. I first receive the address, then I set the DMA-Source pointer to my tx-array (DMA_MemoryBaseAddr). As I have configured autoincrement, several bytes will be transferred. When the second re...

ST-LINK under Windows 8

Posted on October 31, 2012 at 19:26I found the following page useful to permit the installation of the unsigned ST-LINK driver under Windows 8http://www.trickday.com/2012/09/how-to-install-unsigned-drivers-in-windows-8/

How to use CCM RAM on STM32F303VC?

Posted on October 31, 2012 at 12:58There's no examplo using CCM RAM on the STM32F303 stantard library. I need to know how modify the EWARM liker icf file to add the CCM RAM section and how to put an assembler routine in this section.

Asantos by Senior
  • 806 Views
  • 1 replies
  • 0 kudos

SPI1 in DMA2 on STM32F4

Posted on October 29, 2012 at 15:16Hi,I'm trying to switch SPI1 to DMA mode. First I just try to enable on RX channel only, but I tried both RX TX, and many configuration, and I can't figure why it doesn't want to start... #define NBR_BYTES_ 15 uint...

neoirto by Associate II
  • 4281 Views
  • 11 replies
  • 0 kudos

GPIO_PinLockConfig() does not work

Posted on October 29, 2012 at 08:54I have a problem. I set my GPIO port pins on GPIOA. When I wanted to lock them I used GPIO_PinLockConfig function, but when the function passed through. It has done nothing. My pins in LCKR lock register was not lo...

searching for TJpgDec example code

Posted on August 04, 2012 at 15:52hello as the tittle says i'm searching for some example code for http://elm-chan.org/fsw/tjpgd/00index.htmli have fatfs working from chan. i have a display up and running. now i only need to find out how to use the ...

arnold by Associate II
  • 5600 Views
  • 20 replies
  • 0 kudos