STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

need some project advice :)

Posted on October 07, 2012 at 14:21Hello :)I have a little project using a stm32f4 which receives usb data from the pc using the cdc classes (2048bytes @ 60fps) and then draws them to a Plasma dot matrix display.I have it all working ok :) The probl...

russdx by Associate II
  • 2754 Views
  • 13 replies
  • 0 kudos

STM32F2xx and STM32F4xx Demonstration Builder Compile

Posted on November 02, 2012 at 18:18I am having difficulty compiling the Demonstration Builder example code.  I am using MDK-ARM (Keil) with the 256k license but the code is 265k when linked.  I read the app note to disable modules but when I tried ...

wmoyne by Associate II
  • 1502 Views
  • 3 replies
  • 0 kudos

Interrupt priority clarification

Posted on November 02, 2012 at 14:51Hello guys, I have been messing with interrupts recently and I have hard time to find in the manuals how the priorities actually work. I have seen the priority groups and priority values. If I understood it proper...

longchair by Associate III
  • 1496 Views
  • 1 replies
  • 0 kudos

STM32VL Discovery and I2C Accelerometer

Posted on November 02, 2012 at 07:54I need some help setting up I2C connection to LIS302DL or a generic I2C accelerometer. I need some code examples to get the accelerometer working. Thanks in advance.

peppea82 by Associate II
  • 1312 Views
  • 2 replies
  • 0 kudos

STM32F4xx peripheral to memory max rate

Posted on November 01, 2012 at 18:35I have a peripheral bursting 8-bit parallel data at 56MHz gated by a data valid signal. Can the STM32F4xx support peripheral to memory dma at this rate? What is the max rate the STM32F4 can handle dma requests? ...

denny23 by Associate
  • 1339 Views
  • 2 replies
  • 0 kudos

STM32F4Discovery and extra PHY

Posted on November 01, 2012 at 20:17Hello, I am trying to attach external PHY chip to my STM32F4Discovery board. I am using the 'stm32f4x7_eth_lwip' example from the ST site. I think for people that have the bigger evaluation board with already sold...

M0NKA by Senior
  • 747 Views
  • 0 replies
  • 0 kudos

StdPeriphLib Question

Posted on November 01, 2012 at 17:29So does the whole family of STM32M0-STM32M4 have their own StdPeriphDriver offering?  Under the advisement of my hardware guide, I am trying to test out the Freescale Freedom board after I have developed on the ST...

wbarkley by Associate II
  • 709 Views
  • 0 replies
  • 0 kudos

Bus Fault occured randomly during normal operation

Posted on November 01, 2012 at 07:44Dear all, MCU we are using is STM32 F103CBT6, on a motor driver application. Wehave encountered a strange phenomenon that Bus Fault occurred randomly duringnormal operation, and the fault message shows that the PC...

edison72 by Associate
  • 1071 Views
  • 1 replies
  • 0 kudos

DMA: Reset hidden increment registers

Posted on October 31, 2012 at 08:05I emulate an I2C eeprom. I first receive the address, then I set the DMA-Source pointer to my tx-array (DMA_MemoryBaseAddr). As I have configured autoincrement, several bytes will be transferred. When the second re...

ST-LINK under Windows 8

Posted on October 31, 2012 at 19:26I found the following page useful to permit the installation of the unsigned ST-LINK driver under Windows 8http://www.trickday.com/2012/09/how-to-install-unsigned-drivers-in-windows-8/