STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO Sest-Change doesnt get reflected in BSRR

Posted on November 07, 2012 at 09:17Hello All, I am using STM32F2 series. I want to set PORT E pin 1, And here goes my code GPIO_InitTypeDef *GPIO_InitStruct;  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);  GPIO_InitStruct->GPIO_Pin = GPIO_P...

ADC with multiple interrupts

Posted on October 26, 2012 at 09:46Is it possible to have more than one ADC interrupt source? Because I am trying to program ADC3 so that the interrupt can be caused both from an end of conversion (EOC) event and from the analogue watchdog (AWD) eve...

terence-b by Associate II
  • 2862 Views
  • 9 replies
  • 0 kudos

STM32W108 Zigbee Pro stack

Posted on October 16, 2012 at 13:13It appears that the EmberZNet Zigbee Pro stack for the STM32W108 has been withdrawn. The product brief for the STM32W-RFCKIT lists it as supported, but the revision history of the user guide explicitly states that ...

iic with stm32f100

Posted on October 28, 2012 at 12:52Hello, i'm trying to access a compas modul with my stm32F100 (ST32VLDiscovery). I'm trying to do that directly accessing the registers. I think writing the data is ok, but reading doesn't work. I send the start, th...

EXTI on PC3 rising edge only : pull-down ?

Posted on November 07, 2012 at 12:53Hi all,One question about EXTI : I have to trigger an external interrupt on pin PC3 of my STM32F405RG.So I have to configure EXTI3 for rising edge, but is it a good practice to enable pull down to avoid false trig...

neoirto by Associate II
  • 691 Views
  • 0 replies
  • 0 kudos

CAN BUS

Posted on November 06, 2012 at 13:12Hi,I was looking for an example of a CAN BUS for STM32F4 can you help?

orn by Associate II
  • 1370 Views
  • 3 replies
  • 0 kudos

STM32 communicate with MIPI RFFE interface.

Posted on November 05, 2012 at 23:47I am thining of to use STM32 to communicate with MIPI interface. Please see the typical format in the attachment. It is hard to do that with PIC18F controller, for data rate up to 26MHz; by-directional TX/RX SPI l...

Unable to set OVER8 in STM3240G-EVAL (STM32F407IGH6)

Posted on November 05, 2012 at 08:21Hello Friends, Am trying to achieve a high baud rate using USART1 - 7.3728Mbps SYSCLK=168MHz APB2=84MHz Now to achieve this baud rate, I need the OVER8=1 (3 bits for Fraction) Using example code, I set the OVER8 b...

Bootloader version

Posted on November 05, 2012 at 15:09Hello, I have these information written on the stm32f105 micrcontroller STM32F105 VCT6        Z 990TD   93 MYS 99 045 I have read that it depends on the date code of the microcontroller which is 045 in my case. Wh...

hisham23 by Associate III
  • 2849 Views
  • 6 replies
  • 0 kudos