STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with stm32f100c6 clock configuration

Posted on July 16, 2012 at 19:50Hi everybody! I'm using STM32F100C6 with IAR Embedded Workbench IDE and i'm trying to configure the system clock. First i tried to use the external oscillator HSE that's built on the board, 20MHz, here's the code rela...

Discovery-F3 and Discovery-F4 Difference Articles

Posted on November 17, 2012 at 00:13I have written two articles that you may find helpful if you are trying to decide between the STM32 F3 or F4 microcontrollers for a project. Or between the Discovery-F3 and the Discovery-F4 modules. The first arti...

kornak by Associate II
  • 3200 Views
  • 0 replies
  • 0 kudos

Storing image and wave file on SD card

Posted on November 16, 2012 at 06:06How to store image or wav file on SD card (without using FATFS) ...i m using SDIO interface, Keil development environment and discovery board I m done with sd card initialization and single block read write functi...

aambreen by Associate II
  • 735 Views
  • 0 replies
  • 0 kudos

stm32 link utility: core is held in reset

Posted on November 15, 2012 at 18:53First i had problems with the ST-Link drivers, then I had success with installing them. Now I get ''core is held in reset'' error in st-link utility.How to fix this? My only idea is that I shorted something when I...

blaz by Associate
  • 1505 Views
  • 1 replies
  • 0 kudos

Stuck in IRQ handler mode under GDB ? (STM32L152-EVAL)

Posted on November 15, 2012 at 19:33Hello,I am new to debugging on the STM32 and I have a STM32L152-EVAL board and I am trying to bring up the new open source version of RTX on this board.  My setup is as follows.This is setup on a Mac running Mount...

jack23 by Associate
  • 840 Views
  • 0 replies
  • 0 kudos

Power-On Reset from Code?

Posted on November 15, 2012 at 17:01Hey Folks, I know it is possible to reset processor with NVIC_SystemReset(). However, is it possible to enforce a _full_ power-off -> power-on reset from inside the code? Cheers

an by Associate II
  • 1024 Views
  • 1 replies
  • 0 kudos

STM32F4Discovery, I2c vs Exti0

Posted on November 11, 2012 at 18:12Is there an inherent reason why activating EXTI0 using PA0 would interfere with a previously functioning I2C1 transmission operation?  (Atollic TrueStudion Lite) That is, I tried to add ext interrupt from previous...

pccmd by Associate II
  • 2998 Views
  • 7 replies
  • 0 kudos

STM32vldiscovery and hd44780 display

Posted on October 31, 2012 at 20:26Hi, i tried to use IAR example about LCD for use my display hd44780. I connected 6 pin (RS,E,DB4,DB5,DB6,DB7) for use it on 4bit configuration (i'm sure that the connection is good cause i used that on my old ardui...

stm32 uart rtc timer

Posted on November 12, 2012 at 02:43Hello,i need help about designing a stm32 project. Thought is follows. (i must not use any RTOS)1. my stm32100 will handle uart interrupt randomly2. my RTC on stm32 will be updated each 1 second in the rtc interru...

irmakci by Associate II
  • 3982 Views
  • 7 replies
  • 0 kudos

Tim interrupt?

Posted on November 12, 2012 at 17:22I need that display that I put on my stm32f4 Discovery is updated every second, I thought to do so through an interrupt TIM, but I do not know how to configure to work as TIM clock! can you give me some suggestion...

orn by Associate II
  • 1910 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.