lcmuller
Associate II
since
2018-07-19
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About lcmuller
Options
Report User
User Activity
Posts
Replies
STM32 loop strangeness?
2011-03-21
Posted on March 21, 2011 at 19:10STM32 loop strangeness?
STM32 and UART Problem (EIA-485)
2011-03-18
Posted on March 18, 2011 at 18:50STM32 and UART Problem (EIA-485)
Re: STM32 loop strangeness?
2011-05-17
Posted on May 17, 2011 at 14:29I might also add that both arrays are of type uint8_t ...
Re: STM32 and UART Problem (EIA-485)
2011-05-17
Posted on May 17, 2011 at 14:28 That was it! Thanks Clive I didnt think twice when I saw the half-dulpex command in the example since the MAX485 chip works in half duplex mode. Will learn me to read the reference manual in more depth.