STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM

Posted on November 19, 2012 at 10:06What is the main difference between MII and RMII #lmgtfy

VCP for STM32F4_Discovery

Posted on June 22, 2012 at 17:47I have recently downloaded the latest USB libraries which include a virtual comms port project. However all the examples use the ''Eval'' boards which include an LCD etc. rather than the Discovery board which does not...

STM32F4x DMA question

Posted on November 16, 2012 at 14:37In the reference manual at paragraph 9.3.2 (pg 215) is described that the base address for the transfert is stored in DMA_SxPAR o DMA_SxM0AR register. Then in paragraph 9.3.7 (pg 221) is described the possibility ...

stm32f4 discovery n00b/debug question

Posted on November 18, 2012 at 15:55Sorry if this is a repost that I missed but I'm looking to play with one of these boards to practice porting RTOS's to such as uCOS II/III.  But I don't know much about the debug capabilities provided by STLINK/V2...

pauls931 by Associate
  • 2312 Views
  • 4 replies
  • 0 kudos

Remap ADC

Posted on November 17, 2012 at 16:54Hi,Maybe a dumb question but....Would it be possible to remap like 6 inputs of ADC1 to other pins? (stm32f4discovery)I just found some info regarding the remapping of can etc. and i couldn't find theinfo for ADC1....

kenny__84 by Associate II
  • 2431 Views
  • 4 replies
  • 0 kudos

printf and sprintf why it should not be used?

Posted on November 17, 2012 at 12:09To print the result of the ADC on my LCD (16x2) I use the following actions:sprintf(Sprint,''%d'',ADC3ConvertedValue[0]);LCD_PrintData(Sprint, lenght(Sprint)); //  length (Sprint) returns the size of the carrier S...

orn by Associate II
  • 4060 Views
  • 3 replies
  • 0 kudos

STM32F4 Pins and Modules Configure software

Posted on November 17, 2012 at 06:38STM32F4?????????,?????C????. Functions: 1 Pins assignment and  pins confliction indication. 2 making ''C'' program for all modules. Future functions: 3 make program for other modules, eg, watchdog  module,DMA modu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.