STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tim 2 does not work well stm32f4 ... why?

Posted on November 21, 2012 at 15:37 I'm using the following code to update an output device, in this case the LCD, but when I enable TIM 2 the microcontroller stops working! what is wrong? void Tim2_LCD_IT(void){ TIM_TimeBaseInitType...

orn by Associate II
  • 1409 Views
  • 2 replies
  • 0 kudos

STM3210B-EVAL dfu bootloader bin

Posted on November 13, 2012 at 09:11Hi, im searching the compiled dfu bootloader as bin or hex for my STM3210B-EVALMB542 board version B-01 - used for flashing via com port STMicroelectronics flash loader.exe. Could someone send me this file? thank...

STM32L-Discovery hex file

Posted on November 21, 2012 at 02:55Hi all. I've bought a STM32L-Discovery kit. I want to get the original hex file in the microcontroller STM32l152RB on that kit. Please tell me how? Thanks all in advance.

hoang by Associate
  • 1053 Views
  • 1 replies
  • 0 kudos

STM32F417: DCMI HSYNC signal / dead pin (?)

Posted on November 20, 2012 at 18:31Hello,I've spent several days working on getting the DCMI interface on my custom STM32F147 board working. I'm able to configure my camera sensor (OV7725) via I2C and I'm also getting the VSYNC signals from the sen...

ARM PID code in F4 DSP Lib, referring to F1 and F2

Posted on October 30, 2012 at 09:46Hi, I see in the DSP section of the Firmware for the F4, at the following location \STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Libraries\CMSIS\DSP_Lib\Source\ControllerFunctions that there is reference to hardware and sof...

ahiggins9 by Associate II
  • 2891 Views
  • 5 replies
  • 0 kudos

STM

Posted on November 19, 2012 at 10:06What is the main difference between MII and RMII #lmgtfy