STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4Discovery not working without external power?

Posted on November 23, 2012 at 14:34hello,my stm32f4discovery board started not working without connecting external 0-5V power supply to GND and 5V pins.when i plug usb only, nothing happens, none of the leds light. if i connect external power addit...

eraycanli by Associate II
  • 1310 Views
  • 3 replies
  • 0 kudos

what is _impure _ptr ? why am I getting this error ?

Posted on November 22, 2012 at 21:53hello forum I am trying to compile a C program for STM32F4 microcontroller with Eclipse + yagarto compiler I get the error;undefined reference to `_impure_ptr' there is no function ''impure_ptr'' in whole project...

PC host <-> STM32 communication, looking for advices

Posted on November 23, 2012 at 13:52Hi For future projects, I'm looking for the most easy to deploy and foolproof way to communicate between a STM32-based system (mostly L1, some F1) and a PC host. There seems to be 4 ways (Ethernet is not available...

I2S and variable sampling rate

Posted on November 22, 2012 at 13:53Hello, I have fully working I2S with external codec (TLV320AIC23). I have decided to save a crystal and feed the clock to the codec from the I2C pll. So according to the codec pdf this clock needs to be constant (...

M0NKA by Senior
  • 4748 Views
  • 7 replies
  • 0 kudos

SD Command Timeout after SD TX FIFO underrun

Posted on November 22, 2012 at 17:33Sometimes, when writing single blocks to the SD-Card, the TX FIFO underruns and generates an error. If this happens I want to write the block again immediately. Before the block is written, I do a CMD16 command (S...

Moritz M by Associate II
  • 819 Views
  • 0 replies
  • 0 kudos

SD Command Timeout

Posted on July 27, 2012 at 02:58Just curious if any one else has issues with, or has a workaround for an issue I've been experiencing with the SDIO controller on STM32F20x devices.I'm developing a data logging that writes data to SD card at the rate...

carl2399 by Associate III
  • 3007 Views
  • 4 replies
  • 0 kudos

STM32l152-VB _Start up

Posted on November 14, 2012 at 11:40Hello,i need helpWhen debugging my code ,,there is an infinite loop at start up section,,,although i did all clk configurationFor example@file    system_stm32l1xx.c  /* Wait till HSE is ready and if Time out is re...