STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Low level PWM problems

Posted on January 05, 2013 at 01:51 I'm trying to implement PWM on TIM4_CH4 with output on PD15 using only low level register writes as I don't much care for all the high level functions provided. However, I tried to convert the functions to the...

STM32F4xx TIM7 Stopping

Posted on January 04, 2013 at 09:13I want to use TIM6 and TIM7 together . TIM6- Update Event - 2MHz  priority 0x10 TIM7- Update Event - 1MHz priority 0x00 when I closed TIM6 , TIM7 is running normally and toggling LED from PD14 but when I enabled T...

STM32F373 Bootloader

Posted on December 13, 2012 at 05:05I've built a small breakout board for the STM32F373CC:http://ebrombaugh.studionebula.com/embedded/stm32f373breakout/index.htmlI was hoping to be able to use BOOT mode to load it up via the USB device port, but I c...

STM32F100xx TIM4 PWM woes

Posted on January 04, 2013 at 16:58Ok, I'm confused.. according to the docs I should be able to program TIM4 as a PWM with unremaped output on PB9.  However, the Timer API call TIM_CtrlPWMOutputs() has an assert which indicates that TIM4 isn't suppo...

eaverill by Associate II
  • 1377 Views
  • 3 replies
  • 0 kudos

USB CDC Class Driver

Posted on January 02, 2013 at 12:00Hi All,is this normal ? Using 103F along with ST USB CDC Libs on my board and it seems that the USB driver on the PC negotiates a new COM port for every new board i connect to the PC.Normally this is not a problem ...

Accessing SD card via SPI

Posted on January 03, 2013 at 05:56Hi, I have an STM32F4 discovery board and I want to access SD card via SPI. The reason why I want to access Sd card via SPI is that the breakout module that I have has an SPI interface. I have looked on the interne...

osama by Associate II
  • 5599 Views
  • 6 replies
  • 0 kudos

STM32F207 Uart polarity

Posted on January 02, 2013 at 15:55Hi, is there any possibility to change the polarity TX and RX of USART5? I.e. normally idle state is high, startbit is low. We need (due to bad specs of a foreign device) the opposite polarity (software only soluti...

zabel by Associate III
  • 2967 Views
  • 5 replies
  • 0 kudos

How to make your board recognised in dfu mode

Posted on November 05, 2012 at 15:06Hello, I read stm documentation on how to enter a microcontroller into dfu mode Iam using stm32f105, and below are the steps that i did 1- Boot0=1, Boot1= 0 2-PD6 = PA10 = PB5 = 0 3- make reset 4- connect the boar...

hisham23 by Associate III
  • 2184 Views
  • 2 replies
  • 0 kudos

PLL implementation

Posted on January 03, 2013 at 11:46Hi <3 Happy New Year 2013 <3 I want to implement PLL (Phase-locked loop) in STM32F4 Descovery Card The Goal is to control output system frequency to be equal to the input frequency., to eliminate the noise eff...

0690X00000603G1QAI.jpg
bmwael1 by Associate II
  • 914 Views
  • 1 replies
  • 0 kudos

STM32F4 interrupt issue

Posted on January 02, 2013 at 15:29Hello experts, I'm using stm32f4 discovery board. I have connected an interrupt line from a RTC chip to PA1 of my board. The RTC chip gives interrupt signals each 1 second. The way I enable interrupts is as follows...

tybandara by Associate II
  • 1779 Views
  • 3 replies
  • 0 kudos