cancel
Showing results for 
Search instead for 
Did you mean: 

DMA to SPI NDTR Problem

jeffrey2399
Associate
Posted on September 01, 2011 at 17:14

I'm noticing a strange issue when I enable a DMA stream to SPI where the NDTR register changes from my value to 0xFFFF.

Below is a code snippet for the DMA transfer function:

    //Setup DMA for TX

    DMA2_S3PAR = 0x4001300C;

    DMA2_S3M0AR = (uint32)&tx_pkt->preamble;

    DMA2_S3NDTR = tx_pkt->length + CC1120_TX_PKT_OVERHEAD;

    

    //Enable DMA stream

    DMA2_S3CR_bit.EN = 0;

    while( DMA2_S3CR_bit.EN != 0 );

    DMA2_S3CR_bit.EN = 1;

    SPI1_CR2_bit.TXDMAEN = 1;

***As soon as I execute this the NDTR register changes to 0xFFFF

I have confirmed that the NDTR register for the stream is correctly loaded with my length value, but when I enable TXDMA in the SPI peripheral for some reason the NDTR register is set to 0xFFFF.  The DMA stream does work, and I can see the correct SPI TX data, but since the NDTR is changed to 0xFFFF the length of the stream is incorrect.

Has anyone seen this behavior before?

Also for reference below is my DMA stream init routine:

void stm32_dma2_ch3_init( void )

{

    //SPI1 TX - DMA2 Stream3 Channel3

    DMA2_S3CR_bit.EN = 0;

    while( DMA2_S3CR_bit.EN != 0 );

    //Enable DMA2 clock

    RCC_AHB1ENR_bit.DMA2EN = 1;

    

    //DMA Channel3

    DMA2_S3CR_bit.CHSEL = 3;

    //Highest Priority

    DMA2_S3CR_bit.PL = 3;

    

    //Memory and Peripheral Data Size 8-bit

    DMA2_S3CR_bit.MSIZE = 0;

    DMA2_S3CR_bit.PSIZE = 0;

    //Memory increment mode + 1

    DMA2_S3CR_bit.MINC = 1;

    //Peripheral increment mode fixed

    DMA2_S3CR_bit.PINC = 0;

    //Data transfer direction, Memory to Peripheral

    DMA2_S3CR_bit.DIR = 1;

    //Peripheral Flow Control - The peripheral is the flow controller

    DMA2_S3CR_bit.PFCTRL = 1;

    //Transfer Complete Interrupt Enable

    DMA2_S3CR_bit.TCIE = 1;

    

    //Enable DMA2 interrupts ( NVIC_DMA2_CH3 = 59 )

    SETENA1_bit.SETENA59 = 1;

}

#spi #dma
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
infoinfo989
Associate III
Posted on September 01, 2011 at 19:26

Might be because you've set the peripheral as the flow controller.

jeffrey2399
Associate
Posted on September 01, 2011 at 19:33

Is that incorrect?  In this setup the SPI is a slave, so I figured since the clock source for the SPI is external I would need the SPI peripheral to be the flow controller.