STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMStudio maximum sample rate

Posted on January 08, 2013 at 14:42 I have tried a STM Studio, yersteady downloaded. For sample rates less than 100ms are not shown all steps. Is it possible to show steps smaller than 100ms, how and how small they can be? I use an example deliv...

stst9184 by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos

First program not working .

Posted on January 09, 2013 at 13:01I am trying to falsh a example program through a STM32 discovery debugger/programmer on an external STM32 chip. all the connections are right and done according to the instructions written in the Datasheet of STM d...

kunal5959 by Associate II
  • 2049 Views
  • 4 replies
  • 0 kudos

SW Code of DMX512 LED light control in STM32F103

Posted on January 09, 2013 at 02:49from ST documents PDF (LED light control using DMX512 control method ), it mention the application source (IDE IAR Embedded Workbench) is available only on request and is covered by license agreement. So, Can someo...

0690X000006052aQAA.png
tomchen by Associate
  • 1005 Views
  • 0 replies
  • 0 kudos

STM32F4 Discovery FSMC problem

Posted on January 08, 2013 at 03:18I am trying to get the F4 discovery board to communicate with a FPGA board via the FSMC but I am having some problems. I have connected the data 0-15 lines, we, oe, and addr 16-23 from the discovery to my fpga. I c...

networking STM32s

Posted on January 08, 2013 at 20:31I have a question.  I need to connect 2 to 6 STM32s together.  I have motors I need to collectively control with a human machine interface.  Each motor will be controlled by one STM32.  The HMI also needs a STM32. ...

drobison by Associate II
  • 1028 Views
  • 2 replies
  • 0 kudos

LCD_8bits

Posted on December 12, 2012 at 10:09I am trying to use an LCD HD44780 (2X40) with STM3210C-eval. I want to configure it for 8 bits mode. #re-inventing-the-wheel

aymen by Associate II
  • 7093 Views
  • 33 replies
  • 0 kudos

STM32F207 I2C DMA and NAK

Posted on January 08, 2013 at 15:38I am using DMA to transfer data to/from an EEPROM over I2C. Most of the time this is working fine but on the odd occasion when reading from the EEPROM the I2C peripheral does not seem to be sending a NACK when the ...

STM32F4 I2C

Posted on January 04, 2013 at 07:37HiI am attempting to interface the aptina mt9d111 with the stm3240g-eval board.To initialize all the cam registers, I have to make use of I2C. As far as I know I2C sends only 8-bit data. But some of the registers a...

nakulrao by Associate II
  • 2105 Views
  • 4 replies
  • 0 kudos