cancel
Showing results for 
Search instead for 
Did you mean: 

Fatal error: Failed to read CPUID for Cortex device

pradp
Associate II
Posted on July 08, 2011 at 08:37

I am using

Micro controller: STM32F103RCT6TR

IDE: IAR Embedded workbench

Debugger: J-Link ARM  

When I burn it I am getting this error

TotalIRLen = ?, IRPrint = 0x..000000000000000000000011

Fatal error: Failed to read CPUID for Cortex device   Session aborted!

Can anyone help me?

Thank you,

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
rosarium
Associate II
Posted on July 08, 2011 at 19:10

did u select the right device as the target device in the IAR project options.

pradp
Associate II
Posted on July 11, 2011 at 06:40

did you set the proper device as the target at?

For this Micro controller: STM32F103RCT6TR

I am using ST STM32F10xxC as my target

 

which version IAR are you using???

IAR 6.20, J-Link 4.28

rosarium
Associate II
Posted on July 11, 2011 at 09:34

did you copy intrinsics.h at  

C:\Program Files\IAR Systems\Embedded Workbench 6.0\arm\inc\c

if not find here attachde the file and copy it to the path above.