cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f10x_stdperiph_lib warning

raptorhal2
Lead
Posted on July 10, 2011 at 22:56

In my IAR EWARM version 6.20 STM32 library, both stm32f10x_rcc.c and stm32f10x_dma.c have duplicate #define FLAG_Mask statements, producing a warning at compile time.

I redefined the RCC statement and its usage to RCC_FLAG_Mask and all is well. Redefining the DMA statement and all DMA usage to DMA_FLAG_Mask will reduce the probability of application code tripping on the same warning.

This probably occurs on other development IDEs as well.

Cheers, Hal
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
rosarium
Associate II
Posted on July 11, 2011 at 10:16

copy teh attached file at the following path and see if teh warnings are removed.

C:\Program Files\IAR Systems\Embedded Workbench 6.0\arm\inc\c

________________

Attachments :

intrinsics.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzgv&d=%2Fa%2F0X0000000beT%2FpsOj20vkB29P3xt.dVEWf3.YiATIA6ko5Ub5N.gKHj0&asPdf=false
raptorhal2
Lead
Posted on July 11, 2011 at 16:54

I already have revision 43377 of intrinsics.h at that location. Your revision is 34635. Is there some reason to change to your revision ?

My standard peripheral library version is 3.1.2. The ST web site now has version 3.5.0, and it also has the duplicate #defines. Since only a warning is produced, the code may execute OK, but even warnings should be fixed.

ST-One - what say you ?