STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L discovery I can not load program from Keil

Posted on May 14, 2013 at 17:31I have 3 STM32L152 discovery which anser ''Unknown target connected'' when I load a program from keil.I try  setting BOOT0 HIGH when I push the  reset Button .There no result.Best regardsYves de Brest

yves2399 by Associate II
  • 978 Views
  • 1 replies
  • 0 kudos

Playback PCM audio file

Posted on May 13, 2013 at 11:19Hi, I am trying to playback a file with short PCM data recorded at 8KHz, 16bits, mono. I have tryed to configure the I2S with ''I2S_Standard_PCMShort'' but I can�t hear any sound. I have made a file like the file ''aud...

rafael23 by Associate II
  • 3271 Views
  • 5 replies
  • 0 kudos

USART interrupt problem

Posted on May 13, 2013 at 11:10Hi guys, i've a problem with USART communication using interrupts.Using only USART device, the communication works correctly.When i try to using the usart device with some other timers interrupt routines with timers ab...

pietro2 by Associate II
  • 1782 Views
  • 3 replies
  • 0 kudos

Why is the IrDA Baudrate limited to 115.2kBd?

Posted on May 13, 2013 at 20:56Hi, in STM32F4 RM 26.3.12 it says, that ''USART supports only bit rates up to 115.2kBps for the SIR ENDEC''. Can anyone tell me the reason? (115.2kBd must be an increibly low data rate for a 168MHz processor). In fact ...

flyer31 by Senior
  • 1935 Views
  • 5 replies
  • 0 kudos

I2s USART conflict??

Posted on May 13, 2013 at 00:12I am successfully using I2C control and I2S to send data to the CS43L22 and producing simple sawtooth--> musical notes(see http://www.mind-dump.net/configuring-the-stm32f4-discovery-for-audio#comment-1344). When I try ...

pccmd by Associate II
  • 1588 Views
  • 3 replies
  • 0 kudos

STM32F4Discovery FAT FS

Posted on May 04, 2013 at 06:01I am trying to implement at FAT FS on the STM32F4 Discovery board...the firmware package provided by st supplies third party files.  But are these files enough to implement the FAT FS on the STM32F4 board? Or is there ...

ADC via dma and USART

Posted on February 13, 2013 at 10:52 Hello, i am having trouble writing code on STM32F4Discovery. my goal is to get values from ADC in continuous mode and send them to USART/UART (with DMA or without)using interrupts. so i wrote a code made out ...

Continuous data reading from USART

Posted on May 13, 2013 at 00:53Hello,I have a USART data that comes from another device that runs continuously, I have to read all of this data and send it directly to a PC host through a USB.The problem is that I don't want to loose any received da...

slachist by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

STM32F4 running hot

Posted on May 11, 2013 at 10:43hello my sth32f4 discovery is mcu is running hot and u1 is hot also what is going on??