cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 USB Changing Endpoint

mgruen
Associate
Posted on September 01, 2012 at 09:48

Hi,

i currently try to change the endpoint of a demo application from e.g. EP1 to EP2. After changing there is no communication anymore. While debugging i find out, that the fifo of EP2 was set to 0 (in the core configuration) that means no buffer free. I changed this to 128 and the data are copied to the fifo buffer but there is still no transaction. Does anybody konw which additional changes have to be done for a proper working of EP2 (or EP3) instead of EP1 ?

Best regards,

himan
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 01, 2012 at 16:18

Change all references including those in the descriptors.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..