STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with USB lib

Posted on July 29, 2013 at 16:07Hi, I am testing the usb lib 4.0.0 for the VCP functionality on STM32L15xVB targets with 1.3.1 drvier on Win7 hosts. I tried two tests with both usart bridge and loop back examples and unfortunately seeing the same is...

cemer by Associate II
  • 1409 Views
  • 3 replies
  • 0 kudos

Stm32f4 tim7 interrupt problem

Posted on July 26, 2013 at 16:48 Hi 2All! I'm trying to toggle LED with TIM7 interrupt. I'm using STM32f417VG with Coocox CoIDE Code is here: void TIM7Config( void ) { //RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM7,ENABLE); /*TIM7...

M_1 by Associate II
  • 2699 Views
  • 4 replies
  • 0 kudos

Is my understanding of NVIC is correct?

Posted on July 31, 2013 at 22:17Hello, I don't know if my understanding of NVIC is correct especially to System Tick Timer. &sharpinclude ''stm32f10x.h'' void NVIC_Configuration(void)  {           uint32_t priorityGroup;                            ...

STM32F4Discovery - DMA not work.

Posted on July 31, 2013 at 20:14I did try send 100 words 16bits from memory to memory by DMA, and it not work.uint16_t bufor_od[100];  uint16_t bufor_do[100]; RCC->AHB1ENR |= RCC_AHB1ENR_DMA1EN; DMA_InitTypeDef DMA_InitStructure; DMA_DeInit(DMA1_Str...

alprof by Associate II
  • 1444 Views
  • 2 replies
  • 0 kudos

Squarewave out to PF.15

Posted on July 31, 2013 at 05:48Howdy,     Need to output a 25kHz squarewave.  Besides the obvious using a timer ISR, what other ways this can be accomplished? 1. Timer PWM?  As far as I know, no timer can output a PWM out to PF.15.  Am I wrong? 2. ...

bikejog by Associate II
  • 1591 Views
  • 3 replies
  • 0 kudos

help me please about stm32f107 host

Posted on July 26, 2013 at 16:31i make a board with stm32f107 mcu i want to use usb host and read from flash disk. i compile example in st.com an program my chip but not work usb please help me

Timer rising edge

Posted on July 31, 2013 at 08:33Hi,I'm working with stm32f2. I need example code, to count time between two rising edge of GPIO. I read somewhere, that is possibile by appropriate timer's configuration without GPIO's interrupt. Can you help me?Thank...

mosine by Associate II
  • 1249 Views
  • 2 replies
  • 0 kudos

USART and Hyperterminal

Posted on July 31, 2013 at 11:55 Hi, I create on my stm3220G evaluation board an example with USART. The code: #include < stm32f2xx.h > #include < misc.h > // I recommend you have a look at these in the ST firmware folder #include < st...

mosine by Associate II
  • 1168 Views
  • 6 replies
  • 0 kudos

Timer related general questions

Posted on July 31, 2013 at 12:331. What is total delay produced by timer in STM32f205:delay =  (   (ARR+1) * (PSC+1) )  / Timer_freq               or delay =  (   (ARR) * (PSC+1) )  / Timer_freq                   ordelay =  (   (ARR) * (PSC) )  / Ti...

Drive low TIM output in not active state

Posted on July 16, 2013 at 14:24I have STM32F4-discovery board. And I use code from example to configure PWM output. Chapter 14.4.9 TIMx capture/compare enable register (TIMx_CCER) of RM0090:   Bit 0 CC1E: Capture/Compare 1 output enable.     CC1 ch...

glory_man by Associate II
  • 1237 Views
  • 1 replies
  • 0 kudos