cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Virtual Comm port drivers

musatoff
Associate II
Posted on October 14, 2012 at 17:22

Thank you for existence of such driver. But this driver is unsigned. Virtual com port is very useful for many applications. It is very hard to use unsigned drivers for clients. As ST makes any other drivers and signs its, can ST sign virtual com port driver and update installation?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tsuneo
Senior
Posted on October 14, 2012 at 18:12

> It is very hard to use unsigned drivers for clients.

Huh?

Do you sell YOUR device with ST's Vendor ID / Product ID, without ST's sublicense?

ST supposes that YOU should customize the INF file for the VID/PID of YOUR device,

And YOU should get the driver package ''signed''.

Tsuneo

musatoff
Associate II
Posted on October 15, 2012 at 12:20

No, I don't sell system with this driver. I consider possibility of its use. First - is technical questions, second - license. We don't hide that we use chips from ST. Therefore we have no contradiction, as the driver can be used ready from ST. Get own VID/PID and sign driver - is increasing of product design cost.