cancel
Showing results for 
Search instead for 
Did you mean: 

SPI-Flash

ramesh130
Associate II
Posted on August 23, 2010 at 20:09

SPI-Flash

#spi-spi1-remap-pb3
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
kashif
Associate II
Posted on May 17, 2011 at 14:04

i have interfaced AT45DB161. i hv attached the code files (Read/ Write/ Device ID read functions) that might be helpful. change the PIN No.s

pullups are a not a problem. 

tell me if u need more help.

vasilii001
Associate
Posted on October 15, 2012 at 13:05

Were you able to run on SPI1 PB3 - PB5?

Posted on October 15, 2012 at 15:46

Were you able to run on SPI1 PB3 - PB5?

On what part? On the F1 for instance you have to move the JTAG/SWD function off the pins.

This is a very old thread, with a lot of content lost across several forum crashes so don't expect any of the original posters to respond.

This thread deals with the JTAG remapping/disabling

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F107VG PB3 - PB4 - PA15 Alternate Function Usage&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=278

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..