STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Simple Menu example for touch screen

Posted on August 30, 2013 at 16:07 Good afternoon all, I am experimenting with the STM32F4Discovery boards and till now I have managed to interface with pin PC0 by connecting a pot and showing the value of its resistance on the LCD touch screen ...

0690X0000060MnsQAE.gif
philip by Associate
  • 852 Views
  • 0 replies
  • 0 kudos

Flash Loader Demonstrator v2.6.0 bug: RTS line control issue

Posted on August 30, 2013 at 08:34I am using STMFlashLoader.exe on Windows 7 (64bit).RTS Output control in Command line version doesn't work.DTR control works fine.To the STMicroelectronics software designers.  This is obviously bug in theSTMFlashLo...

vvvalka by Associate
  • 673 Views
  • 0 replies
  • 0 kudos

STM32 Timers - Help with TIM_Period

Posted on August 28, 2013 at 12:14Hi,I'm studying the timers on STM32F100 using a STM32VLDISCOVERY board.Per example:  TIM_TimeBaseStructure.TIM_Prescaler = SystemCoreClock/1000 - 1; TIM_TimeBaseStructure.TIM_Period = 1;Will set the count frequency ...

ee06091 by Associate III
  • 1917 Views
  • 3 replies
  • 0 kudos

USB virtual com port for stm32f3discovery

Posted on February 15, 2013 at 19:33Hi,I plan to transfer the gyroscope value to PC through USB virtual com port. So I downloaded the latest version for the USB full speed device library for stm32(version 4.0). However, the projects, specifically th...

vsaaket8 by Associate II
  • 2134 Views
  • 5 replies
  • 0 kudos

Overwriting written flash memory with 0xFFFFFFFF on STM32L

Posted on August 27, 2013 at 20:48I need a reliably method of overwriting flash memory on a STM32L device (STM32L152CB). On the other STM32F series, this was easy, as I could write zeros on top of previously written flash memory contents reliably. T...

mlakata by Associate II
  • 6148 Views
  • 10 replies
  • 1 kudos

I2C3 interrupt not working

Posted on August 29, 2013 at 15:54 Hi all, I have some problems with I2C3 interrupts, I have enabled the interrupt but the handler interrupt never executes. Here is the interrupt configuration: NVIC_InitTypeDef NVIC_InitStru...

edgar by Associate II
  • 770 Views
  • 0 replies
  • 0 kudos

File System

Posted on August 24, 2013 at 13:10I am implementing file system for stm32f407vg controller. I am getting problem in implementing directory next function. can any one help me ?

srinivas by Associate
  • 1499 Views
  • 3 replies
  • 0 kudos