STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151 Signals generator with time shift/delay

Posted on August 28, 2013 at 16:10Hi,I'm trying to generate 3 signal using TIM3&TIM4.the first signal run at 8MHz, DutyCycle 50%, the second signal should run every odd cycles of the first signal and the third should run every even cycles of the fir...

0690X000006051DQAQ.png
tamir by Associate
  • 1670 Views
  • 3 replies
  • 0 kudos

Exiting STOP mode on USART character

Posted on August 30, 2013 at 14:27 Hi, I have a bit of an issue - I'm trying to put an STM32 into STOP mode, but to have it wake up when a character is sent over the USART (and to receive that character). My code is just: // .....

gw by Associate II
  • 1403 Views
  • 3 replies
  • 0 kudos

minimum HCLOK for USB OTG FS

Posted on September 01, 2013 at 09:24I use today HCLK of 120Mhz taken from the systemclk of 120Mhz (prescale by 1), and active USB OTG FS no problem. To save power I want to go as much as possible low with the freq, when not during fast operations, ...

Barbie by Associate II
  • 723 Views
  • 0 replies
  • 0 kudos

I2C on STM32F4 gets stuck while checking EV6 flag

Posted on May 26, 2012 at 10:14 Hi guys, I'm working on a STM32F4 Discovery board and trying send over I2C. Therefore I'm using the functions from the Standard Peripheral Library. Unfortunately the device stucks after sending the address ...

return address of isr

Posted on August 31, 2013 at 20:31hi i am working on stm32f4. i am having a small programming issue, while my code is executing, ISR comes, i want to change the return address of ISR, i.e it does not goes back from where the processor left the code....

bilal by Associate II
  • 1060 Views
  • 1 replies
  • 0 kudos

JavaScript interpreter on STM32 Discovery boards

Posted on February 13, 2013 at 11:34Just to say about a project I've been working on - it's a JavaScript interpreter for the STM32 called Espruino (http://www.espruino.com)It's available for the STM32VL, STM32F3 and STM32F4 boards - as well as some ...

gw by Associate II
  • 789 Views
  • 1 replies
  • 0 kudos

Stm32 Encoder interface

Posted on July 12, 2011 at 11:20Nid help in Stm32 Encoder Interface, to turn the motor in clockwise and anti-clockwise direction. Thanks  #encoder-interface #stm32f0-discovery

Making reserved bits at reset value

Posted on August 31, 2013 at 09:29In many of registers of STM32F205 it is mentioned that reserved bits should be kept ar reset state.Is it sure that reading reserved bits always return its reset value or its undefined. If it is undefined then have t...

programming STM32F0 over UART

Posted on July 08, 2013 at 14:53Hi guys, i need to program a stm32f0 mcu using a serial cable.At this moment i'm using an external St-link device.Can i use only a serial cable without st-link (e.g. over hyper terminal)? #uart

pietro2 by Associate II
  • 5639 Views
  • 10 replies
  • 0 kudos