STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDR_ON errata on LQFP100 for STM32F4

Posted on August 19, 2013 at 23:21A warning so no one else will get caught by this.  On the original STM32F4 design docs pin 99 on LQFP100 is shown as RFU or PDR_ON, and diagrams show it can be connected to Vdd.  The gotcha is this only applies to r...

Debugging Ethernet

Posted on September 14, 2012 at 17:49Hi,I have a new board based on STM32F407 that is wired iin RMII with a  KSZ8031RNL PHY. I would like to port the stm32 f4 eval board sample to my board. I have defined the RMII_MODEHere the maping of the phy     ...

jdumaresq by Associate II
  • 2125 Views
  • 3 replies
  • 0 kudos

Dma -> usart circular buffer questions

Posted on August 29, 2013 at 04:24 I was trying to write out the usart using dma. I thought everything was working till I actually looked at the data. The data seemed to always be wrong so I extracted all the relevant code to test it separately ...

Flash/Program memory Increase

Posted on September 02, 2013 at 16:21Hi, Sorry this might be a stupid question as I have not done enough research. But if some one could answer will save me lot of time. Is there a way I can increase the program memory of STM32f407 using external f...

STM32F4 I2C issues

Posted on September 01, 2013 at 18:26Hello, I am trying to get the I2C bus to run with the MMA8452 accelerometer, but it just wont. I can generate a start condition but nothing else. I'm watching the bus lines with a scope/logic analyzer and I can s...

totally by Associate II
  • 1771 Views
  • 3 replies
  • 0 kudos

Stm32f4 ADC exemple

Posted on August 31, 2013 at 19:50hello i tried ST's adc exemple and i got weird values of my variable while debugging , for exemple i got 30 for 2.0 v and -1000 for 2.5 v , so anyone have a working code with no weird things? and thnx :)

help - F103 window watchdog

Posted on August 31, 2013 at 21:45 hello dear forum, I am trying to setup window watchdog on F103 I want wwdg to be reset in a window of 8 - 12 milisecond I set wwdg prescaler to 2 so wwdg timer is counting every 0.227 microsecon...

STM32L151 Signals generator with time shift/delay

Posted on August 28, 2013 at 16:10Hi,I'm trying to generate 3 signal using TIM3&TIM4.the first signal run at 8MHz, DutyCycle 50%, the second signal should run every odd cycles of the first signal and the third should run every even cycles of the fir...

0690X000006051DQAQ.png
tamir by Associate
  • 1673 Views
  • 3 replies
  • 0 kudos

Exiting STOP mode on USART character

Posted on August 30, 2013 at 14:27 Hi, I have a bit of an issue - I'm trying to put an STM32 into STOP mode, but to have it wake up when a character is sent over the USART (and to receive that character). My code is just: // .....

gw by Associate II
  • 1406 Views
  • 3 replies
  • 0 kudos