cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery VCP Problem

taha_najmee
Associate II
Posted on October 29, 2012 at 01:55

Hello,

I am trying to add VCP on STM32F4Discovery but have some issues which I am not able to figure out.

When I add this command

USBD_Init(&USB_OTG_dev, USB_OTG_FS_CORE_ID, &USR_desc, &USBD_CDC_cb, &USR_cb);

in main, it stops working. I tried to debug it using Keil and found out that it stops somewhere in the Reset_Handler code in startup_stm32f4xx.s file. It stops somewhere before going into the main() routine.

Did anybody have similar kind of problem? I will really appreciate if someone can guide me through it. 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on October 29, 2012 at 02:37

This code is not in that execution path. Take a look a system_stm32f4xx.c and SystemInit().

Turn off the ''run to main'' and step the debugger through the start up code.

You could also use the STM3240G-EVAL project as the basis of your code, and make sure your settings (HSE, PLL, USB48) in system_stm32f4xx.c reflect the fact the discovery board uses an 8 MHz external crystal, not 25 MHz, and make sure the value is HSE_VALUE is correctly defined.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
taha_najmee
Associate II
Posted on October 29, 2012 at 18:42

Thanks for the reply ... My HSE Value is already 8MHz, but I didn't know that I have to change values for PLL and USB48. So those value should be 8MHz as well or something different?

Reset_Handler    PROC

        EXPORT  Reset_Handler             [WEAK]

        IMPORT  SystemInit

        IMPORT  __main

                 LDR     R0, =SystemInit

                 BLX     R0

                 LDR     R0, =__main

                 BX      R0

                 ENDP

While debugging the code I observed that it executes the LDR R0, =__main but it goes somewhere after executing BX R0. I am not sure where it jumps to because the execution arrow is no where to be found on Keil after that particular instruction. 

Posted on October 29, 2012 at 20:02

Press the Stop button, or add some breakpoints.

__main is Keil's C runtime startup code, it should be clearing out the static allocations, and copying initialized data, prior to calling your main() function.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..