STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

mistake in stm32f4xx.h

Posted on November 16, 2013 at 17:31to be migrated, sourceId: 35463:697285D7-A9CA-445D-B16C-F23BF0E3B1A3 #stm32f4

SYSCLK

Posted on November 16, 2013 at 17:00I read in system_stm32f4xx.c that after reset, sysclk is 168MHz. I want to creat a function delay 1s.void Delay(void) { uint32_t i; for(i=0; i<0xA037A00; ++i)   // A037A00 = 168.000.000 { }   }.Who can explain fo...

41003160 by Associate II
  • 1608 Views
  • 3 replies
  • 0 kudos

Timer 5 never counts from zero

Posted on November 16, 2013 at 05:57 #define SYS_CLK 24000000 /* in this example we use SPEED_HIGH = 24 MHz */ #define DELAY_TIM_FREQUENCY 1000000 /* = 1MHZ -> timer runs in microseconds */ /* Enable timer clock - use TIMER5 */ RCC_APB1PeriphC...

stm32f103rb NSS

Posted on November 15, 2013 at 02:58hello,I have a problem about the stm32f103rb. According to the RM0008  reference manual downloaded in your website, I find the description of  slave select(NSS) pin management. So the NSS signal can be driven high...

wwtzh2013 by Associate II
  • 1782 Views
  • 3 replies
  • 0 kudos

USART communicatoin with DMA

Posted on November 15, 2013 at 19:30The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F4 FreeRTOS and us accuracy delay

Posted on November 13, 2013 at 13:07Hi everyone, I'm currently working on a musical (using midi) project on which i need very precise delay in order to synchronise with other instruments. This delay should be able to be accurate at 1 microsecond. Fo...

benoit2 by Associate II
  • 2594 Views
  • 2 replies
  • 0 kudos

DAC & ADC speed help

Posted on November 12, 2013 at 15:54 Hello, I'm coding a real time system based on STM32F427 requiring a lot of ressources and using almost all peripherials (ADC, DAC, SPI, I2aC, USART, USB, SDIO). This is why I want to reduce the ressou...

SPI slave using DMA on STM32F405RG

Posted on November 15, 2013 at 10:31I am working on the SPI communication between PC and STM32F405RG MCU. FTDI chip FT232H serves as a bridge between PC and MCU (USB to SPI converter). FTDI is set to be SPI master and MCU is slave. I am using DMA tr...

milos by Associate
  • 890 Views
  • 0 replies
  • 0 kudos