cancel
Showing results for 
Search instead for 
Did you mean: 

ASSERT error in STM32F37xx eval samples

mk
Associate II
Posted on January 03, 2013 at 08:49

We have an STM32373C-EVAL board and we've been trying out the firmware demo samples. One thing I've noticed is that if I enable the USE_FULL_ASSERT, most samples will crash. (Well, not crash but get caught in the assert trap.)

Eg. in the ''STM32F3xx_AN4045_V1.0.0'' (STM32F3xx_IAP), the following will crash:

...

if (STM_EVAL_PBGetState(BUTTON_KEY)  == 0x00)

...

(Only if you push the button though.)

and

...

FLASH_If_Init();

...

Is this normal? Should I just disable the USE_FULL_ASSERT and forget about it or is there somewhere where I should submit a bug report?

#don't-rush-to-claim-a-bug #stm32f37xx-eval
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
yayi
Associate II
Posted on January 03, 2013 at 09:55

Hello, I am not sure about what's the problem but :

If you use FULL_ASSERT, you need this code : For me it is present on every example and it works.

#ifdef  USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *   where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

Good Luck.

We have an STM32373C-EVAL board and we've been trying out the firmware demo samples. One thing I've noticed is that if I enable the USE_FULL_ASSERT, most samples will crash. (Well, not crash but get caught in the assert trap.)

Eg. in the ''STM32F3xx_AN4045_V1.0.0'' (STM32F3xx_IAP), the following will crash:

...

if (STM_EVAL_PBGetState(BUTTON_KEY)  == 0x00)

...

(Only if you push the button though.)

and

...

FLASH_If_Init();

...

Is this normal? Should I just disable the USE_FULL_ASSERT and forget about it or is there somewhere where I should submit a bug report?
frankmeyer9
Associate II
Posted on January 03, 2013 at 11:14

The ASSERT macro as found in ST's examples has the same purpose as the Clib functio/macro

assert

. It is used to catch states/expressions which are syntactically correct, but not semantically. In the ST example code, this macro is often used to catch incorrect or meaningless parameters. (I know it from the Discovery firmware and example code, not having an EVAL board).

If ST's example code fails such assertions, it is buggy.

Seems it was released in a hurry, without thorough testing.

If the code works correctly without the USE_FULL_ASSERT, the expectation of the developer had been wrong in this case.

mk
Associate II
Posted on January 04, 2013 at 10:31

Yes, that was what I thought as well.

Do you know somewhere where I can submit this bug report?

frankmeyer9
Associate II
Posted on January 04, 2013 at 11:11

Do you know somewhere where I can submit this bug report?

 

Not really.

In open-source applications, you often find ''submit bug reports to ...'' in the release notes. I've found nothing like that yet in any ST firmware.

Not sure if they are actually interested ...

Maybe you can make some rattling noise, to catch the attention of a ST moderator like ST-One ;)

Andrew Neil
Super User
Posted on January 04, 2013 at 12:36

''Do you know somewhere where I can submit this bug report?''

First, you would have to clearly demonstrate that it really is a bug

http://www.catb.org/~esr/faqs/smart-questions.html#idp29846432

Are you sure  that you are using the code entirely  unmodified, and have correctly configured your project?

Have you stepped through the code to see exactly why it is ASSERTing?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mk
Associate II
Posted on January 04, 2013 at 13:29

That's why I was asking whether this behavior is to be expected.

And yes, I'm sure that the code is entirely unmodified. And I haven't configured the project in any way, besides adding the USE_FULL_ASSERT. It comes preconfigured from ST. (Two mcu builds are available. I've selected the stm32f37x.) Everything seems to work ... but not when adding the USE_FULL_ASSERT.

Amel NASRI
ST Employee
Posted on January 21, 2013 at 16:45

Hi Morten,

Did you tried to build your own example based on the StandardPeriphLibrary for F3 board or even the ST examples other than the IAP one?

Best Regards,

ST MCU

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.