STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f4Discovery I2C Problem

Posted on March 25, 2012 at 16:57 Hello everyone, I'am new to arm based processors but I have already worked with the Atmel Mega family. I am using Atollic True Studio and thedeliveredstandardlibrary. I try to read the LSM303DLH (ma...

Number of external interrupts available

Posted on November 27, 2013 at 09:24HiI'm currently using EXTI0 to EXTI4 already. When I configure EXTI5 and above, I have an error when setting it in the NVIC, since EXTI5_IRQn and above are not defined in stm32f4xx.h.From the Reference manual I go...

terence-b by Associate II
  • 3080 Views
  • 6 replies
  • 0 kudos

How to set up communication between PC?

Posted on December 01, 2013 at 20:21I have an old STM32 Value Line Discovery Kit. Never used since now. I'm looking to set up communication between PC? Is it possible? I googled around and found this and that about people messing around something ca...

ivarbug by Associate
  • 1233 Views
  • 2 replies
  • 0 kudos

linked eroor IAR

Posted on November 29, 2013 at 23:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

tifou by Associate II
  • 1744 Views
  • 2 replies
  • 0 kudos

Branch with link instruction does not jump to SystemInit()

Posted on November 28, 2013 at 19:24Hello,We are a robotics association from ENSEIRB-MATMECA (Bordeaux, France). We are developping some boards and a template project for STM32 devices.One of our boards embed a STM32F103C4 microcontroller. We use th...

kjoly by Associate II
  • 2383 Views
  • 7 replies
  • 0 kudos

USART between PC to STM32f4 discovery

Posted on November 27, 2013 at 15:45I read example in projec example include Lib 1.2.0 . But I can't connect. I open Hyper terminal but no COM from stm32f4. When I connect board stm32f4, it will appear in Universal Serial Bus Controller. How can I c...

41003160 by Associate II
  • 1781 Views
  • 3 replies
  • 0 kudos

Is the st-linkv2 SWJ capable?

Posted on November 27, 2013 at 22:14Hello, i'm working with a custom board with a STM32L151RD and a st-linkv2. For debugging purpose i only have access to SWD pins:SWCLK (PA14) SWDIO (PA13)TRACESWO (PB3)NRSTBut the microcontroller is JTAG wired by d...

STM32F372 first project

Posted on November 28, 2013 at 18:44I am new to ARM and am trying to create my very first project using an STM32F372CC micro. I have a prototype board connected to a STM32L discovery board. I am using Keil uVision V4.70.0.0. I can compile and downlo...

Erratum in errata of STM32F101xC/D/E ?

Posted on November 29, 2013 at 11:53ES0104: STM32F101xC/D/E and STM32F103xC/D/E high-density device limitationsIn CD00197763 �2.13.1 it is statedClear ADDR by reading SR1 register followed by reading SR3SR3? Not SR2? I assume this is an erratum in t...

hendrik2 by Associate II
  • 1565 Views
  • 2 replies
  • 0 kudos

emWin library problem

Posted on November 27, 2013 at 08:30Hello,I tried to build on Atollic the precompiled package around the emWin graphical lib(AN4323).I build for STM322xG-EVAL, but I get two errors:c:/program files (x86)/atollic/truestudio for arm pro 3.3.0/armtools...

pcu by Associate II
  • 1521 Views
  • 2 replies
  • 0 kudos