User Activity

Posted on July 10, 2013 at 09:39I want to get STM32CONTINUAUSB , I find the marketing status is proposal, so what does it mean? How can I get it?
Posted on April 28, 2013 at 07:51Hello,        I want to use UART + DMA to receive unknown length packet. So I tried to use IDLE interrupt to monitor the end of the packet. On the other hand, I use a PC tools to send several bytes data and delay a w...
Posted on April 22, 2013 at 11:40Hello,         I modify the demo code in STM32L1xx_StdPeriph_Lib_V1.2.0 --> TIM --> OCToggle. I reconfigured the TIM3_CH3 CCR3_Val to 40 to generate 200KHz square waveform. The output frequency measured is only 122Hz...
Posted on April 18, 2013 at 17:42As the subject described, could I use TIM3 CH3 in input capture mode to measure a frequency, and at the same time use TIM3 CH4 in output compare mode to generate a PWM signal?
Posted on April 15, 2013 at 09:53RM0038: TS: Trigger selection can only selected to TI1FP1 or TI2FP2. However, how to connect this two input to TIM3 CHANNEL 4?