STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 USB communication

Posted on March 07, 2014 at 17:27Hi Hi, I have done some test using the USART1 PA9 and PA10 pin to communicate with my arduino board, i made some basic configuration like this : USART_InitTypeDef USART1_Init;RCC_APB2PeriphClockCmd(RCC_APB2Periph_USA...

jean2 by Associate II
  • 1306 Views
  • 1 replies
  • 0 kudos

CAN Filter configuration

Posted on March 05, 2014 at 13:17Hello guys,Can anyone explain me how CAN filters work? I cannot understand the reference manual, I don�t know if I am stupid or it is very bad explained (stm32f407).I read a lot of post on the internet but I have a m...

The solution for a 800×480 LCD based on STM32

Posted on March 07, 2014 at 10:40Hi everyone,    I'd like to choise STM32 for a HMI case, whoes main requirement was a TFT LCD of 800*480. There were 2 idea: 1) STM32F1 + RA7785 2) STM32F429 Which was the better? Everybody could give me some suggest...

albhuang by Associate II
  • 736 Views
  • 1 replies
  • 0 kudos

Stm32 LIN driver

Posted on November 07, 2013 at 16:50 Hello everybody. I need to use LIN communication with stm32 mikrocontroller. I see the std lib have function for lin communication, but the comments in the usart.c file is strange. The lin communi...

totti001 by Associate II
  • 1267 Views
  • 1 replies
  • 0 kudos

STM32F401 USB without HSE

Posted on March 05, 2014 at 12:59I'm looking at making a device with the STM32F401, and I'm wondering if USB on it can function without a HSE crystal?The clock diagrams seem to imply that PLL48 can work off of HSI, but the reference implies that USB...

gw by Associate II
  • 2643 Views
  • 5 replies
  • 0 kudos

Change the speed of GPIO

Posted on March 06, 2014 at 12:41Hi there, I want to change the speed of GPIO for STM32f4 discovery board. The maximun speed I can get on specified pin is 6 MHz and I want to get 20 Mhz. we know that the discovery board has external clock circuit to...

ali2003a by Associate II
  • 2177 Views
  • 6 replies
  • 0 kudos

Reset of Timer

Posted on March 07, 2014 at 03:15 Hi , I have a timer programmed to monitor a timeout event using timer interrupt(every 100ms). If the event occurs within the time (100ms) i would like to refresh the timeout. Is the below code a...

stm32f405, help on jtag programming

Posted on March 06, 2014 at 00:08Dear all, i am trying to program a stm32f405 just soldered on a prototype pcb. Seems jtag TAP is accesible, but for some reason i cannot halt the cpu: Open On-Chip Debugger 0.7.0 (2013-08-04-10:13) Licensed under GNU...

Angelo1 by Associate II
  • 1483 Views
  • 2 replies
  • 0 kudos